Hi evrybody
I am building the WL18xx software:
lyudmila@lyudmila-linuxmint ~/wl8-build_Point9-6 $ git clone git://git.ti.com/wilink8-wlan/build-utilites.git
Клонирование в «build-utilites»…
remote: Counting objects: 928, done.
remote: Compressing objects: 100% (452/452), done.
remote: Total 928 (delta 509), reused 761 (delta 456)
Получение объектов: 100% (928/928), 12.83 MiB | 2.38 MiB/s, готово.
Определение изменений: 100% (509/509), готово.
Проверка соединения… готово.
lyudmila@lyudmila-linuxmint ~/wl8-build_Point9-6 $ cd build-utilites
lyudmila@lyudmila-linuxmint ~/wl8-build_Point9-6/build-utilites $ ./build_wl18xx.sh init
Changing ROOTFS path to /media/lyudmila/rfs
Using user defined kernel
Makefile was found. Kernel version was set to 4.4.139.
***** initializing workspace (w/o build) *****
Cloning into: kernel
Cloning into: openssl
Клонирование в «/home/lyudmila/wl8-build_Point9-6/build-utilites/src/openssl»…
fatal: unable to connect to github.com:
github.com[0: 140.82.121.3]: errno=Время ожидания соединения истекло
Cloning into: libnl
Клонирование в «/home/lyudmila/wl8-build_Point9-6/build-utilites/src/libnl»…
fatal: unable to connect to github.com:
github.com[0: 140.82.121.4]: errno=Время ожидания соединения истекло
All other packages are cloned successfully.
What's wrong? Why are openssl and libnl not cloned?
setup-env file contents:
# \\\//
# -(o o)-
#========================oOO==(_)==OOo=======================
# This file contains the exports needed for automating the
# build process of WLAN components.
# Place this file in the same directory with wl18xx_build.sh
# build scripts. No need to run 'source setup-env', the build
# scripts will perfom it internaly.
#===========================================================
# User specific environment settings - use full PATH
# if DEFAULT toolchain path is set toolchain will be downloaded to ./toolchain.
export TOOLCHAIN_PATH=/home/lyudmila/timesysPoint9-6/twr_vf600/toolchain/bin
# if DEFAULT path to root filesystem is set ./fs folder will be used.
#export ROOTFS=/home/lyudmila/timesysPoint9-6/twr_vf600/kernel-source/linux-4.4/rfs
export ROOTFS=/media/lyudmila/rfs
#if DEFAULT kernel path is set - kernel will be downloaded (set branch to match kernel version)
export KERNEL_PATH=/home/lyudmila/timesysPoint9-6/twr_vf600/kernel-source/linux-4.4
# if KERNEL_VARIANT below is set the build script will look for kernel specific
# patches under the patches directory:
# - patches under the pathces/driver_patches/$KERNEL_VARIANT directory would be
# applied during "modules" build.
# - patches under the patches/kernel_patches/$/$KERNEL_VARIANT directory would
# be applied to the kernel pointed by KERNEL_PATH in case the "patch_kernel"
# command is used.
# Note: the kernel is not built automatically after the patches are applied
export KERNEL_VARIANT=4.4.139-ts-armv7l
export CROSS_COMPILE=armv7l-timesys-linux-gnueabi-
export ARCH=arm
[ "$TOOLCHAIN_PATH" != "DEFAULT" ] && export PATH=$TOOLCHAIN_PATH:$PATH