Other Parts Discussed in Thread: CC3235SF, SYSCONFIG
I am attempting to connect to a HTTP server using a CC3235MODSF running on a custom board. I am getting an error status of -2006 from the call to HTTPClient_connect2. Also, I tried running the httpget demo on my CC3235SF LaunchPad and I am getting the same error of -2006. Here is the output from the httpget demo:
*************************************************
HTTP GET Application
*************************************************
[NETAPP EVENT] IP Acquired: IP=10.123.45.1 , Gateway=10.123.45.1
Sending a HTTP GET request to 'http://www.example.com'
Error! code = -2006, Description = httpTask: connect failed