Hi! I created a test repo on git to see if I could download OTA files. I managed to do so when the repo is set to public, but it only gives an error when it's set to private. Here is the output:
CdnGithub_SendReqDir: uri=/repos/---/TI_OTA_Test/contents/ HttpClient_RecvSkipHdr: http error code HTTP/1.1 404 CdnGithub_ParseRespDir: ERROR HttpClient_RecvSkipHdr, status=-20310 OTA_run: ERROR CdnClient_ReqOtaDir, Status=-20310
I have tried creating a Git Token and inserting it in "otauser.h"->OTA_VENDOR_TOKEN (even tried the base64 format), but this does not work for either public or private (though it gives http errors 403 or 400 depending on the settings). Clearly I'm missing something, but everything works except for the authorization/credentials for the private repo. Thankful for any help I can get!
Kind regards
David