This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WL1807MOD: Maximum current/power consumption for each of the VIO and VBAT rails

Part Number: WL1807MOD


Hi team,

Customer is checking the current/power consumption of WL1807 and would like to know about the following question.

The datasheet(in Table 9-1) says Maximum piak current consumption is 850mA,

  • Is this the combined value of both VBAT and VIO? Or is this the value for VBAT only?
  • If VBAT only, what is the maximum current consumption of VIO?

The datasheet(in 8.3 Recommended Operating Condition) says maximum power dissipation is 2.8W for WLAN operation.

  • Is this the combined value of both VBAT and VIO?
  •  If not, what is the maximum current consumption of each?

Your support is highly appreciated.