Other Parts Discussed in Thread: UNIFLASH, SYSCONFIG, , CC3235SF
Hello,
I'm trying to build your httpget example for the previously mentioned DevBoard. In the stage of the makefile where the SLImageCreator builds the image (*.sli file) i get exactly the same error as here (https://e2e.ti.com/support/wireless-connectivity/wi-fi-group/wifi/f/wi-fi-forum/967859/failed-to-build-image-to-flash-the-board). Next i tried the network terminal example and i also got the same error. So i assume that the error is not related to a specific example. Even when i call the SLImageCreator from the command line without any arguments, i got this error. Thus I am pretty sure that it is a problem with the SLImageCreator in generell. Since you provide this tool also with the UniFlash application, i installed UniFlash aswell. When i call the SLImageCreator from UniFlash, it works. This leads me to the assumption that my environment (OS, dependencies,...) is not the problem. I temporally fixed the error by replacing the imagecreator folder within the Simple Link by the imagecreator folder from UniFlash. But this does not look like a reasonable solution to me. I hope you can reproduce my error and find a solution for the problem. If you need more detailed information from me, please do not hesitate to ask me.
My setup is:
Ubuntu 22.04
Code Composer Studio 12.4.0.00007
Simple Link CC32XX SDK 7.10.0.13
SysConfig 1.16.2
UniFlash 8.3.0
Many thanks in advance!
Tobias