This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
After the cc3301 successfully connects to the AP, restarting the cc3301 and attempting to reconnect to the AP results in the first connection attempt failing, while the second connection attempt succeeds.
The reason for the first connection failure is that the AP sends a disassociation packet, which happens very quickly, but we do not receive any related events and have to wait until the connection times out.
The second connection may also fail, as the firmware no longer responds to commands issued by the driver, the firmware logs no longer show any prints, while under normal circumstances, the firmware logs would continuously display prints. This error occurs with a high probability.
so, My issue is:
1. Why doesn't the driver receive the disassociation event in a timely manner?
2. Why does such a connection operation cause the firmware to stop working?
Hello,
Can we please get some wireshark captures, and firmware logs?
In order to capture Firmware logs you need to download the simplelink WiFi toolbox https://www.ti.com/tool/SIMPLELINK-WIFI-TOOLBOX
Follow the Logger instructions on the application and provide us with the data collected.
Thanks,
Hi AB
Here is log, connect failed, and receive event HINT_FW_DOWNLOAD_ERROR,
wifi connect test101 abcdef1234 -r
ssid: test101, len 7
key: abcdef1234, len 10, index 0
bssid:
0000 00 00 00 00 00 00
security: -1, wepauthtype: -1
chanspec 0
0000 00 00 00 00 00 00 00 00 - 00 00 00 00 00 00 00 00
0010 00 00 00 00 00 00 00 00 - 00 00 00 00 00 00 00 00
scan_security: 0, scan_encryption: 0
[WLAN EVENT] Device disconnected from the AP, ReasonCode: 1
Easycam network link is off!!
Do reconnect...
clean prev pmk
libwifi_connect
scan 4 find ssid test101 (len 7)
security type: WPA3
[WLAN EVENT] Device disconnected from the AP, ReasonCode: 200
connect to test101, sectype: 12
Get unexpected event: HINT_FW_DOWNLOAD_ERROR
connect timeout
connect to test101, sectype: 12
wlan_connect faild, return 1078428372
can not find test101
scan test101 failed
WIFI Connect 0th Retry Fail.
[ERROR]: Wifi Connect Fail!!
Hi,
The log is not using the correct parser so the interesting packets are not decodable.
If you are using R5, the firmware version is 1.7.0.185. You need to use the logger.bin file from the R5 itself (under cc33xx_mcu_package_R5\tools\wifi_fw).
What logger.bin are you using?
Shlomi
the logger.bin I used is from simplelink_wifi_toolbox_2_2_5/radio-tool/binaries/CC3301/logger.bin.
I can't find any logger.bin file in cc33xx_mcu_package_R5, please provide it, and also provide a sample of log which you want.
BTW, how to get the fw version?
Hi,
the logger that is embedded in toolbox 2_2_5 is newer.
you can open the cc33xx_fw.bin in hex and look for cc33xx_ and you should see the firmware version.
for example, on 2_2_5 you get 1.7.0.188.
On R5, the firmware should be under cc33xx_mcu_package_R5\tools\wifi_fw as I mentioned earlier.
The version is 1.7.0.185.
Shlomi
I know where is the firmware, but where is the logger.bin you mentioned? I can't find it in cc33xx_mcu_package_R5\tools\wifi_fw.
what should I do?
Oh, sorry for that, I simply copied it locally to this directory. can you use the attached?
Hi,
I will take it internally with R&D.
Can you please share the AP vendor and model? we want to see if we have it in-house.
Thanks,
Shlomi