This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Murata wifi/BT module LBEE5ZSTNC-523 and production calibration

We are currently preparing production using Murata Wifi/BT module and we would like to know if we need to do calibration on every module in our production process ??

it is require to run nvs calibration for every individual unit that we ship?  And is this to tweak power settings so that the units are more consistent in their Tx power and Rx sensitivity?  So if calibration were not performed on each unit, some units would have potentially lower wifi performance?

if we are require to perform calibration on every unit, then does a wifi external antenna need to be attached during calibration?  Or is it something internal in the chip?

Just trying to understand in detail what is required and what the impacts are.

Thanks,

  • Hello,

    The NVS maps the PA curve in dBm to mV using the power detector in the FEM (Front End Module). Each PA curve is different so unique NVS is needed per device.

    There are 2 options, getting NVS from Murata per module assuming they executed the process in the module production or generate it by yourself.

    You can also use a default NVS for all your product but then TI can't promise the output power accuracy.

    Regards,

    Eran 

  • sound like we will have to do the calibration process for every unit we build in production if we want the best performance.

    what about connecting the external  antenna before running calibration, is this require ?

    thanks

  • Hello,

    This is required because generating the NVS needs 50ohm termination.

    Regards

    Eran 

  • Eran,

     

    is it possible I send you an email directly regarding Bluetooth setup from our FCC lab ??

    Thanks

  • Hello,

    Please indicate the customer name and location. I will connect you with one of my team member to help you locally.

    Thanks

    Eran

  • Hi,

    I prefer continue supporting over the E2E. it gives us better tracking on the quality of service our customers getting and also support our community.

    Regarding the BT FCC tools, you should use HCI. did you get TI Wirelss tool kit?

    Do you get support from TI local office in your area?

    Regards,

    Eran

  • 3348.FCC-BT.docx

     

    our product is current at the FCC lab and attached are some BT questions the lab is asking.   can you please comments.

     

    Thanks

     

  • Hi,

    you should use the HCI command HCI_VS_DRPb_Tester_Con_TX. on the left side of the HCI tool you may see parameters to control the modulation (EDR3, EDR2, GFSK, BLE and CW). You don't need to use the hopping command because the FCC should be tested in single channel and the hopping is taken as a factor.1616.SWRU136 - HCITester User Guide.pdf

    please find attached HCI user guide.

    As for BT system, it’s being tested according to FCC 15.247(a)

    See the following explanation for BT correction factor calculation:

     

    • Up to 5 slots of transmission
    • Hopping rate of 1600 hops/sec
    • Maximum dwell time is: 5/1600 sec or 3.125 msec
    • Maximum dwell time in a 100 msec period is 4 * 3.125 msec = 12.5 msec
    • Therefore, the average correction factor is 20log(12.5/100) = -18dB
    • As this is a hopping ratio, the correction factor can be applied to the average value of the signal provided the average value was measured with the device continuously transmitting

     Regards,

    Eran

  • The Murata wifi/BT module is connected directly to an embedded ARM9 CPU running Linux.    Do you have any information for Linux ??

     

    Thanks

  • Hi,

    You may use the opcode to execute the same using Linux.

    Regards,

    Eran

  • do you have any Linux examples that you can share ?

     

    Thanks

  • Any comments or feedback regarding Linux examples that you can share ??

     

    Thanks

  • Hi,

    I assume you are using Linux with Bluez support, hcitool is bluez utility, so you can use the same command to validate. Let me know if i have understood you question correctly.

    Thanks

    Vijay

  • Yes we are using BlueZ and yes we do have Linux hcitool.   What I am looking for is the exact or actual hcitool commands that I can provide to the FCC lab in order for them to perform the Bluetooth tests and certification

     

    Thanks

     

  • Hi

    http://linuxcommand.org/man_pages/hcitool1.htm
    please use the below command to configure the packet type

     cc [--role=m|s] [--pkt-type=<ptype>] <bdaddr>
                  Create baseband  connection  to  remote  device  with  Bluetooth
                  address  bdaddr.   Option --pkt-type specifies a list of allowed
                  packet types.  <ptype>  is  a  comma-separated  list  of  packet
                  types,  where  the possible packet types are DM1, DM3, DM5, DH1,
                  DH3, DH5, HV1, HV2, HV3.  Default is to allow all packet  types.
                  Option  --role  can have value m (do not allow role switch, stay
                  master) or s (allow role switch, become slave if the  peer  asks
                  to become master). Default is m.
    
    
    
    Thanks
    Vijay
  • <html xmlns:v="urn:schemas-microsoft-com:vml"
    xmlns:o="urn:schemas-microsoft-com:office:office"
    xmlns:w="urn:schemas-microsoft-com:office:word"
    xmlns:m="http://schemas.microsoft.com/office/2004/12/omml"
    xmlns="http://www.w3.org/TR/REC-html40">
    
    <head>
    <meta http-equiv=Content-Type content="text/html; charset=shift_jis">
    <meta name=ProgId content=Word.Document>
    <meta name=Generator content="Microsoft Word 12">
    <meta name=Originator content="Microsoft Word 12">
    <link rel=File-List href="Bluetooth%20link%20issue_files/filelist.xml">
    <link rel=Edit-Time-Data href="Bluetooth%20link%20issue_files/editdata.mso">
    <!--[if !mso]>
    <style>
    v\:* {behavior:url(#default#VML);}
    o\:* {behavior:url(#default#VML);}
    w\:* {behavior:url(#default#VML);}
    .shape {behavior:url(#default#VML);}
    </style>
    <![endif]--><!--[if gte mso 9]><xml>
     <o:DocumentProperties>
      <o:Author>admin</o:Author>
      <o:Template>NormalEmail.dotm</o:Template>
      <o:LastAuthor>admin</o:LastAuthor>
      <o:Revision>2</o:Revision>
      <o:TotalTime>2</o:TotalTime>
      <o:Created>2013-02-07T17:58:00Z</o:Created>
      <o:LastSaved>2013-02-07T19:33:00Z</o:LastSaved>
      <o:Pages>2</o:Pages>
      <o:Words>157</o:Words>
      <o:Characters>896</o:Characters>
      <o:Lines>7</o:Lines>
      <o:Paragraphs>2</o:Paragraphs>
      <o:CharactersWithSpaces>1051</o:CharactersWithSpaces>
      <o:Version>12.00</o:Version>
     </o:DocumentProperties>
    </xml><![endif]-->
    <link rel=themeData href="Bluetooth%20link%20issue_files/themedata.thmx">
    <link rel=colorSchemeMapping
    href="Bluetooth%20link%20issue_files/colorschememapping.xml">
    <!--[if gte mso 9]><xml>
     <w:WordDocument>
      <w:Zoom>90</w:Zoom>
      <w:SpellingState>Clean</w:SpellingState>
      <w:GrammarState>Clean</w:GrammarState>
      <w:TrackMoves>false</w:TrackMoves>
      <w:TrackFormatting/>
      <w:ValidateAgainstSchemas/>
      <w:SaveIfXMLInvalid>false</w:SaveIfXMLInvalid>
      <w:IgnoreMixedContent>false</w:IgnoreMixedContent>
      <w:AlwaysShowPlaceholderText>false</w:AlwaysShowPlaceholderText>
      <w:DoNotPromoteQF/>
      <w:LidThemeOther>EN-US</w:LidThemeOther>
      <w:LidThemeAsian>X-NONE</w:LidThemeAsian>
      <w:LidThemeComplexScript>X-NONE</w:LidThemeComplexScript>
      <w:Compatibility>
       <w:DoNotExpandShiftReturn/>
       <w:BreakWrappedTables/>
       <w:SnapToGridInCell/>
       <w:WrapTextWithPunct/>
       <w:UseAsianBreakRules/>
       <w:DontGrowAutofit/>
       <w:SplitPgBreakAndParaMark/>
       <w:DontVertAlignCellWithSp/>
       <w:DontBreakConstrainedForcedTables/>
       <w:DontVertAlignInTxbx/>
       <w:Word11KerningPairs/>
       <w:CachedColBalance/>
       <w:UseFELayout/>
      </w:Compatibility>
      <w:BrowserLevel>MicrosoftInternetExplorer4</w:BrowserLevel>
      <m:mathPr>
       <m:mathFont m:val="Cambria Math"/>
       <m:brkBin m:val="before"/>
       <m:brkBinSub m:val="&#45;-"/>
       <m:smallFrac m:val="off"/>
       <m:dispDef/>
       <m:lMargin m:val="0"/>
       <m:rMargin m:val="0"/>
       <m:defJc m:val="centerGroup"/>
       <m:wrapIndent m:val="1440"/>
       <m:intLim m:val="subSup"/>
       <m:naryLim m:val="undOvr"/>
      </m:mathPr></w:WordDocument>
    </xml><![endif]--><!--[if gte mso 9]><xml>
     <w:LatentStyles DefLockedState="false" DefUnhideWhenUsed="true"
      DefSemiHidden="true" DefQFormat="false" DefPriority="99"
      LatentStyleCount="267">
      <w:LsdException Locked="false" Priority="0" SemiHidden="false"
       UnhideWhenUsed="false" QFormat="true" Name="Normal"/>
      <w:LsdException Locked="false" Priority="9" SemiHidden="false"
       UnhideWhenUsed="false" QFormat="true" Name="heading 1"/>
      <w:LsdException Locked="false" Priority="9" QFormat="true" Name="heading 2"/>
      <w:LsdException Locked="false" Priority="9" QFormat="true" Name="heading 3"/>
      <w:LsdException Locked="false" Priority="9" QFormat="true" Name="heading 4"/>
      <w:LsdException Locked="false" Priority="9" QFormat="true" Name="heading 5"/>
      <w:LsdException Locked="false" Priority="9" QFormat="true" Name="heading 6"/>
      <w:LsdException Locked="false" Priority="9" QFormat="true" Name="heading 7"/>
      <w:LsdException Locked="false" Priority="9" QFormat="true" Name="heading 8"/>
      <w:LsdException Locked="false" Priority="9" QFormat="true" Name="heading 9"/>
      <w:LsdException Locked="false" Priority="39" Name="toc 1"/>
      <w:LsdException Locked="false" Priority="39" Name="toc 2"/>
      <w:LsdException Locked="false" Priority="39" Name="toc 3"/>
      <w:LsdException Locked="false" Priority="39" Name="toc 4"/>
      <w:LsdException Locked="false" Priority="39" Name="toc 5"/>
      <w:LsdException Locked="false" Priority="39" Name="toc 6"/>
      <w:LsdException Locked="false" Priority="39" Name="toc 7"/>
      <w:LsdException Locked="false" Priority="39" Name="toc 8"/>
      <w:LsdException Locked="false" Priority="39" Name="toc 9"/>
      <w:LsdException Locked="false" Priority="35" QFormat="true" Name="caption"/>
      <w:LsdException Locked="false" Priority="10" SemiHidden="false"
       UnhideWhenUsed="false" QFormat="true" Name="Title"/>
      <w:LsdException Locked="false" Priority="1" Name="Default Paragraph Font"/>
      <w:LsdException Locked="false" Priority="11" SemiHidden="false"
       UnhideWhenUsed="false" QFormat="true" Name="Subtitle"/>
      <w:LsdException Locked="false" Priority="22" SemiHidden="false"
       UnhideWhenUsed="false" QFormat="true" Name="Strong"/>
      <w:LsdException Locked="false" Priority="20" SemiHidden="false"
       UnhideWhenUsed="false" QFormat="true" Name="Emphasis"/>
      <w:LsdException Locked="false" Priority="59" SemiHidden="false"
       UnhideWhenUsed="false" Name="Table Grid"/>
      <w:LsdException Locked="false" UnhideWhenUsed="false" Name="Placeholder Text"/>
      <w:LsdException Locked="false" Priority="1" SemiHidden="false"
       UnhideWhenUsed="false" QFormat="true" Name="No Spacing"/>
      <w:LsdException Locked="false" Priority="60" SemiHidden="false"
       UnhideWhenUsed="false" Name="Light Shading"/>
      <w:LsdException Locked="false" Priority="61" SemiHidden="false"
       UnhideWhenUsed="false" Name="Light List"/>
      <w:LsdException Locked="false" Priority="62" SemiHidden="false"
       UnhideWhenUsed="false" Name="Light Grid"/>
      <w:LsdException Locked="false" Priority="63" SemiHidden="false"
       UnhideWhenUsed="false" Name="Medium Shading 1"/>
      <w:LsdException Locked="false" Priority="64" SemiHidden="false"
       UnhideWhenUsed="false" Name="Medium Shading 2"/>
      <w:LsdException Locked="false" Priority="65" SemiHidden="false"
       UnhideWhenUsed="false" Name="Medium List 1"/>
      <w:LsdException Locked="false" Priority="66" SemiHidden="false"
       UnhideWhenUsed="false" Name="Medium List 2"/>
      <w:LsdException Locked="false" Priority="67" SemiHidden="false"
       UnhideWhenUsed="false" Name="Medium Grid 1"/>
      <w:LsdException Locked="false" Priority="68" SemiHidden="false"
       UnhideWhenUsed="false" Name="Medium Grid 2"/>
      <w:LsdException Locked="false" Priority="69" SemiHidden="false"
       UnhideWhenUsed="false" Name="Medium Grid 3"/>
      <w:LsdException Locked="false" Priority="70" SemiHidden="false"
       UnhideWhenUsed="false" Name="Dark List"/>
      <w:LsdException Locked="false" Priority="71" SemiHidden="false"
       UnhideWhenUsed="false" Name="Colorful Shading"/>
      <w:LsdException Locked="false" Priority="72" SemiHidden="false"
       UnhideWhenUsed="false" Name="Colorful List"/>
      <w:LsdException Locked="false" Priority="73" SemiHidden="false"
       UnhideWhenUsed="false" Name="Colorful Grid"/>
      <w:LsdException Locked="false" Priority="60" SemiHidden="false"
       UnhideWhenUsed="false" Name="Light Shading Accent 1"/>
      <w:LsdException Locked="false" Priority="61" SemiHidden="false"
       UnhideWhenUsed="false" Name="Light List Accent 1"/>
      <w:LsdException Locked="false" Priority="62" SemiHidden="false"
       UnhideWhenUsed="false" Name="Light Grid Accent 1"/>
      <w:LsdException Locked="false" Priority="63" SemiHidden="false"
       UnhideWhenUsed="false" Name="Medium Shading 1 Accent 1"/>
      <w:LsdException Locked="false" Priority="64" SemiHidden="false"
       UnhideWhenUsed="false" Name="Medium Shading 2 Accent 1"/>
      <w:LsdException Locked="false" Priority="65" SemiHidden="false"
       UnhideWhenUsed="false" Name="Medium List 1 Accent 1"/>
      <w:LsdException Locked="false" UnhideWhenUsed="false" Name="Revision"/>
      <w:LsdException Locked="false" Priority="34" SemiHidden="false"
       UnhideWhenUsed="false" QFormat="true" Name="List Paragraph"/>
      <w:LsdException Locked="false" Priority="29" SemiHidden="false"
       UnhideWhenUsed="false" QFormat="true" Name="Quote"/>
      <w:LsdException Locked="false" Priority="30" SemiHidden="false"
       UnhideWhenUsed="false" QFormat="true" Name="Intense Quote"/>
      <w:LsdException Locked="false" Priority="66" SemiHidden="false"
       UnhideWhenUsed="false" Name="Medium List 2 Accent 1"/>
      <w:LsdException Locked="false" Priority="67" SemiHidden="false"
       UnhideWhenUsed="false" Name="Medium Grid 1 Accent 1"/>
      <w:LsdException Locked="false" Priority="68" SemiHidden="false"
       UnhideWhenUsed="false" Name="Medium Grid 2 Accent 1"/>
      <w:LsdException Locked="false" Priority="69" SemiHidden="false"
       UnhideWhenUsed="false" Name="Medium Grid 3 Accent 1"/>
      <w:LsdException Locked="false" Priority="70" SemiHidden="false"
       UnhideWhenUsed="false" Name="Dark List Accent 1"/>
      <w:LsdException Locked="false" Priority="71" SemiHidden="false"
       UnhideWhenUsed="false" Name="Colorful Shading Accent 1"/>
      <w:LsdException Locked="false" Priority="72" SemiHidden="false"
       UnhideWhenUsed="false" Name="Colorful List Accent 1"/>
      <w:LsdException Locked="false" Priority="73" SemiHidden="false"
       UnhideWhenUsed="false" Name="Colorful Grid Accent 1"/>
      <w:LsdException Locked="false" Priority="60" SemiHidden="false"
       UnhideWhenUsed="false" Name="Light Shading Accent 2"/>
      <w:LsdException Locked="false" Priority="61" SemiHidden="false"
       UnhideWhenUsed="false" Name="Light List Accent 2"/>
      <w:LsdException Locked="false" Priority="62" SemiHidden="false"
       UnhideWhenUsed="false" Name="Light Grid Accent 2"/>
      <w:LsdException Locked="false" Priority="63" SemiHidden="false"
       UnhideWhenUsed="false" Name="Medium Shading 1 Accent 2"/>
      <w:LsdException Locked="false" Priority="64" SemiHidden="false"
       UnhideWhenUsed="false" Name="Medium Shading 2 Accent 2"/>
      <w:LsdException Locked="false" Priority="65" SemiHidden="false"
       UnhideWhenUsed="false" Name="Medium List 1 Accent 2"/>
      <w:LsdException Locked="false" Priority="66" SemiHidden="false"
       UnhideWhenUsed="false" Name="Medium List 2 Accent 2"/>
      <w:LsdException Locked="false" Priority="67" SemiHidden="false"
       UnhideWhenUsed="false" Name="Medium Grid 1 Accent 2"/>
      <w:LsdException Locked="false" Priority="68" SemiHidden="false"
       UnhideWhenUsed="false" Name="Medium Grid 2 Accent 2"/>
      <w:LsdException Locked="false" Priority="69" SemiHidden="false"
       UnhideWhenUsed="false" Name="Medium Grid 3 Accent 2"/>
      <w:LsdException Locked="false" Priority="70" SemiHidden="false"
       UnhideWhenUsed="false" Name="Dark List Accent 2"/>
      <w:LsdException Locked="false" Priority="71" SemiHidden="false"
       UnhideWhenUsed="false" Name="Colorful Shading Accent 2"/>
      <w:LsdException Locked="false" Priority="72" SemiHidden="false"
       UnhideWhenUsed="false" Name="Colorful List Accent 2"/>
      <w:LsdException Locked="false" Priority="73" SemiHidden="false"
       UnhideWhenUsed="false" Name="Colorful Grid Accent 2"/>
      <w:LsdException Locked="false" Priority="60" SemiHidden="false"
       UnhideWhenUsed="false" Name="Light Shading Accent 3"/>
      <w:LsdException Locked="false" Priority="61" SemiHidden="false"
       UnhideWhenUsed="false" Name="Light List Accent 3"/>
      <w:LsdException Locked="false" Priority="62" SemiHidden="false"
       UnhideWhenUsed="false" Name="Light Grid Accent 3"/>
      <w:LsdException Locked="false" Priority="63" SemiHidden="false"
       UnhideWhenUsed="false" Name="Medium Shading 1 Accent 3"/>
      <w:LsdException Locked="false" Priority="64" SemiHidden="false"
       UnhideWhenUsed="false" Name="Medium Shading 2 Accent 3"/>
      <w:LsdException Locked="false" Priority="65" SemiHidden="false"
       UnhideWhenUsed="false" Name="Medium List 1 Accent 3"/>
      <w:LsdException Locked="false" Priority="66" SemiHidden="false"
       UnhideWhenUsed="false" Name="Medium List 2 Accent 3"/>
      <w:LsdException Locked="false" Priority="67" SemiHidden="false"
       UnhideWhenUsed="false" Name="Medium Grid 1 Accent 3"/>
      <w:LsdException Locked="false" Priority="68" SemiHidden="false"
       UnhideWhenUsed="false" Name="Medium Grid 2 Accent 3"/>
      <w:LsdException Locked="false" Priority="69" SemiHidden="false"
       UnhideWhenUsed="false" Name="Medium Grid 3 Accent 3"/>
      <w:LsdException Locked="false" Priority="70" SemiHidden="false"
       UnhideWhenUsed="false" Name="Dark List Accent 3"/>
      <w:LsdException Locked="false" Priority="71" SemiHidden="false"
       UnhideWhenUsed="false" Name="Colorful Shading Accent 3"/>
      <w:LsdException Locked="false" Priority="72" SemiHidden="false"
       UnhideWhenUsed="false" Name="Colorful List Accent 3"/>
      <w:LsdException Locked="false" Priority="73" SemiHidden="false"
       UnhideWhenUsed="false" Name="Colorful Grid Accent 3"/>
      <w:LsdException Locked="false" Priority="60" SemiHidden="false"
       UnhideWhenUsed="false" Name="Light Shading Accent 4"/>
      <w:LsdException Locked="false" Priority="61" SemiHidden="false"
       UnhideWhenUsed="false" Name="Light List Accent 4"/>
      <w:LsdException Locked="false" Priority="62" SemiHidden="false"
       UnhideWhenUsed="false" Name="Light Grid Accent 4"/>
      <w:LsdException Locked="false" Priority="63" SemiHidden="false"
       UnhideWhenUsed="false" Name="Medium Shading 1 Accent 4"/>
      <w:LsdException Locked="false" Priority="64" SemiHidden="false"
       UnhideWhenUsed="false" Name="Medium Shading 2 Accent 4"/>
      <w:LsdException Locked="false" Priority="65" SemiHidden="false"
       UnhideWhenUsed="false" Name="Medium List 1 Accent 4"/>
      <w:LsdException Locked="false" Priority="66" SemiHidden="false"
       UnhideWhenUsed="false" Name="Medium List 2 Accent 4"/>
      <w:LsdException Locked="false" Priority="67" SemiHidden="false"
       UnhideWhenUsed="false" Name="Medium Grid 1 Accent 4"/>
      <w:LsdException Locked="false" Priority="68" SemiHidden="false"
       UnhideWhenUsed="false" Name="Medium Grid 2 Accent 4"/>
      <w:LsdException Locked="false" Priority="69" SemiHidden="false"
       UnhideWhenUsed="false" Name="Medium Grid 3 Accent 4"/>
      <w:LsdException Locked="false" Priority="70" SemiHidden="false"
       UnhideWhenUsed="false" Name="Dark List Accent 4"/>
      <w:LsdException Locked="false" Priority="71" SemiHidden="false"
       UnhideWhenUsed="false" Name="Colorful Shading Accent 4"/>
      <w:LsdException Locked="false" Priority="72" SemiHidden="false"
       UnhideWhenUsed="false" Name="Colorful List Accent 4"/>
      <w:LsdException Locked="false" Priority="73" SemiHidden="false"
       UnhideWhenUsed="false" Name="Colorful Grid Accent 4"/>
      <w:LsdException Locked="false" Priority="60" SemiHidden="false"
       UnhideWhenUsed="false" Name="Light Shading Accent 5"/>
      <w:LsdException Locked="false" Priority="61" SemiHidden="false"
       UnhideWhenUsed="false" Name="Light List Accent 5"/>
      <w:LsdException Locked="false" Priority="62" SemiHidden="false"
       UnhideWhenUsed="false" Name="Light Grid Accent 5"/>
      <w:LsdException Locked="false" Priority="63" SemiHidden="false"
       UnhideWhenUsed="false" Name="Medium Shading 1 Accent 5"/>
      <w:LsdException Locked="false" Priority="64" SemiHidden="false"
       UnhideWhenUsed="false" Name="Medium Shading 2 Accent 5"/>
      <w:LsdException Locked="false" Priority="65" SemiHidden="false"
       UnhideWhenUsed="false" Name="Medium List 1 Accent 5"/>
      <w:LsdException Locked="false" Priority="66" SemiHidden="false"
       UnhideWhenUsed="false" Name="Medium List 2 Accent 5"/>
      <w:LsdException Locked="false" Priority="67" SemiHidden="false"
       UnhideWhenUsed="false" Name="Medium Grid 1 Accent 5"/>
      <w:LsdException Locked="false" Priority="68" SemiHidden="false"
       UnhideWhenUsed="false" Name="Medium Grid 2 Accent 5"/>
      <w:LsdException Locked="false" Priority="69" SemiHidden="false"
       UnhideWhenUsed="false" Name="Medium Grid 3 Accent 5"/>
      <w:LsdException Locked="false" Priority="70" SemiHidden="false"
       UnhideWhenUsed="false" Name="Dark List Accent 5"/>
      <w:LsdException Locked="false" Priority="71" SemiHidden="false"
       UnhideWhenUsed="false" Name="Colorful Shading Accent 5"/>
      <w:LsdException Locked="false" Priority="72" SemiHidden="false"
       UnhideWhenUsed="false" Name="Colorful List Accent 5"/>
      <w:LsdException Locked="false" Priority="73" SemiHidden="false"
       UnhideWhenUsed="false" Name="Colorful Grid Accent 5"/>
      <w:LsdException Locked="false" Priority="60" SemiHidden="false"
       UnhideWhenUsed="false" Name="Light Shading Accent 6"/>
      <w:LsdException Locked="false" Priority="61" SemiHidden="false"
       UnhideWhenUsed="false" Name="Light List Accent 6"/>
      <w:LsdException Locked="false" Priority="62" SemiHidden="false"
       UnhideWhenUsed="false" Name="Light Grid Accent 6"/>
      <w:LsdException Locked="false" Priority="63" SemiHidden="false"
       UnhideWhenUsed="false" Name="Medium Shading 1 Accent 6"/>
      <w:LsdException Locked="false" Priority="64" SemiHidden="false"
       UnhideWhenUsed="false" Name="Medium Shading 2 Accent 6"/>
      <w:LsdException Locked="false" Priority="65" SemiHidden="false"
       UnhideWhenUsed="false" Name="Medium List 1 Accent 6"/>
      <w:LsdException Locked="false" Priority="66" SemiHidden="false"
       UnhideWhenUsed="false" Name="Medium List 2 Accent 6"/>
      <w:LsdException Locked="false" Priority="67" SemiHidden="false"
       UnhideWhenUsed="false" Name="Medium Grid 1 Accent 6"/>
      <w:LsdException Locked="false" Priority="68" SemiHidden="false"
       UnhideWhenUsed="false" Name="Medium Grid 2 Accent 6"/>
      <w:LsdException Locked="false" Priority="69" SemiHidden="false"
       UnhideWhenUsed="false" Name="Medium Grid 3 Accent 6"/>
      <w:LsdException Locked="false" Priority="70" SemiHidden="false"
       UnhideWhenUsed="false" Name="Dark List Accent 6"/>
      <w:LsdException Locked="false" Priority="71" SemiHidden="false"
       UnhideWhenUsed="false" Name="Colorful Shading Accent 6"/>
      <w:LsdException Locked="false" Priority="72" SemiHidden="false"
       UnhideWhenUsed="false" Name="Colorful List Accent 6"/>
      <w:LsdException Locked="false" Priority="73" SemiHidden="false"
       UnhideWhenUsed="false" Name="Colorful Grid Accent 6"/>
      <w:LsdException Locked="false" Priority="19" SemiHidden="false"
       UnhideWhenUsed="false" QFormat="true" Name="Subtle Emphasis"/>
      <w:LsdException Locked="false" Priority="21" SemiHidden="false"
       UnhideWhenUsed="false" QFormat="true" Name="Intense Emphasis"/>
      <w:LsdException Locked="false" Priority="31" SemiHidden="false"
       UnhideWhenUsed="false" QFormat="true" Name="Subtle Reference"/>
      <w:LsdException Locked="false" Priority="32" SemiHidden="false"
       UnhideWhenUsed="false" QFormat="true" Name="Intense Reference"/>
      <w:LsdException Locked="false" Priority="33" SemiHidden="false"
       UnhideWhenUsed="false" QFormat="true" Name="Book Title"/>
      <w:LsdException Locked="false" Priority="37" Name="Bibliography"/>
      <w:LsdException Locked="false" Priority="39" QFormat="true" Name="TOC Heading"/>
     </w:LatentStyles>
    </xml><![endif]-->
    <style>
    <!--
     /* Font Definitions */
     @font-face
    	{font-family:Wingdings;
    	panose-1:5 0 0 0 0 0 0 0 0 0;
    	mso-font-charset:2;
    	mso-generic-font-family:auto;
    	mso-font-pitch:variable;
    	mso-font-signature:0 268435456 0 0 -2147483648 0;}
    @font-face
    	{font-family:Gulim;
    	panose-1:2 11 6 0 0 1 1 1 1 1;
    	mso-font-alt:Gulim;
    	mso-font-charset:129;
    	mso-generic-font-family:swiss;
    	mso-font-pitch:variable;
    	mso-font-signature:-1342176593 1775729915 48 0 524447 0;}
    @font-face
    	{font-family:"Cambria Math";
    	panose-1:2 4 5 3 5 4 6 3 2 4;
    	mso-font-charset:0;
    	mso-generic-font-family:roman;
    	mso-font-pitch:variable;
    	mso-font-signature:-536870145 1107305727 0 0 415 0;}
    @font-face
    	{font-family:Cambria;
    	panose-1:2 4 5 3 5 4 6 3 2 4;
    	mso-font-charset:0;
    	mso-generic-font-family:roman;
    	mso-font-pitch:variable;
    	mso-font-signature:-536870145 1073743103 0 0 415 0;}
    @font-face
    	{font-family:Calibri;
    	panose-1:2 15 5 2 2 2 4 3 2 4;
    	mso-font-charset:0;
    	mso-generic-font-family:swiss;
    	mso-font-pitch:variable;
    	mso-font-signature:-536870145 1073786111 1 0 415 0;}
    @font-face
    	{font-family:Tahoma;
    	panose-1:2 11 6 4 3 5 4 4 2 4;
    	mso-font-charset:0;
    	mso-generic-font-family:swiss;
    	mso-font-pitch:variable;
    	mso-font-signature:-520081665 -1073717157 41 0 66047 0;}
    @font-face
    	{font-family:"MS PGothic";
    	panose-1:2 11 6 0 7 2 5 8 2 4;
    	mso-font-charset:128;
    	mso-generic-font-family:swiss;
    	mso-font-pitch:variable;
    	mso-font-signature:-536870145 1791491579 18 0 131231 0;}
    @font-face
    	{font-family:"\@Gulim";
    	panose-1:2 11 6 0 0 1 1 1 1 1;
    	mso-font-charset:129;
    	mso-generic-font-family:swiss;
    	mso-font-pitch:variable;
    	mso-font-signature:-1342176593 1775729915 48 0 524447 0;}
    @font-face
    	{font-family:"\@MS PGothic";
    	panose-1:2 11 6 0 7 2 5 8 2 4;
    	mso-font-charset:128;
    	mso-generic-font-family:swiss;
    	mso-font-pitch:variable;
    	mso-font-signature:-536870145 1791491579 18 0 131231 0;}
    @font-face
    	{font-family:"Arial \, sans-serif";
    	mso-font-alt:"Times New Roman";
    	mso-font-charset:0;
    	mso-generic-font-family:auto;
    	mso-font-pitch:auto;
    	mso-font-signature:0 0 0 0 0 0;}
     /* Style Definitions */
     p.MsoNormal, li.MsoNormal, div.MsoNormal
    	{mso-style-unhide:no;
    	mso-style-qformat:yes;
    	mso-style-parent:"";
    	margin:0in;
    	margin-bottom:.0001pt;
    	mso-pagination:widow-orphan;
    	font-size:12.0pt;
    	font-family:"Gulim","sans-serif";
    	mso-bidi-font-family:"MS PGothic";
    	mso-fareast-language:JA;}
    a:link, span.MsoHyperlink
    	{mso-style-noshow:yes;
    	mso-style-priority:99;
    	color:blue;
    	text-decoration:underline;
    	text-underline:single;}
    a:visited, span.MsoHyperlinkFollowed
    	{mso-style-noshow:yes;
    	mso-style-priority:99;
    	color:purple;
    	text-decoration:underline;
    	text-underline:single;}
    p
    	{mso-style-noshow:yes;
    	mso-style-priority:99;
    	mso-margin-top-alt:auto;
    	margin-right:0in;
    	mso-margin-bottom-alt:auto;
    	margin-left:0in;
    	mso-pagination:widow-orphan;
    	font-size:12.0pt;
    	font-family:"Gulim","sans-serif";
    	mso-bidi-font-family:"MS PGothic";
    	mso-fareast-language:JA;}
    p.MsoAcetate, li.MsoAcetate, div.MsoAcetate
    	{mso-style-noshow:yes;
    	mso-style-priority:99;
    	mso-style-link:"Balloon Text Char";
    	margin:0in;
    	margin-bottom:.0001pt;
    	mso-pagination:widow-orphan;
    	font-size:8.0pt;
    	font-family:"Tahoma","sans-serif";
    	mso-fareast-font-family:Gulim;
    	mso-fareast-language:JA;}
    span.BalloonTextChar
    	{mso-style-name:"Balloon Text Char";
    	mso-style-noshow:yes;
    	mso-style-priority:99;
    	mso-style-unhide:no;
    	mso-style-locked:yes;
    	mso-style-link:"Balloon Text";
    	font-family:"Tahoma","sans-serif";
    	mso-ascii-font-family:Tahoma;
    	mso-hansi-font-family:Tahoma;
    	mso-bidi-font-family:Tahoma;}
    span.EmailStyle20
    	{mso-style-type:personal;
    	mso-style-noshow:yes;
    	mso-style-unhide:no;
    	font-family:"Cambria","serif";
    	mso-ascii-font-family:Cambria;
    	mso-hansi-font-family:Cambria;
    	color:#1F497D;}
    span.EmailStyle21
    	{mso-style-type:personal;
    	mso-style-noshow:yes;
    	mso-style-unhide:no;
    	font-family:"Calibri","sans-serif";
    	mso-ascii-font-family:Calibri;
    	mso-hansi-font-family:Calibri;
    	color:#1F497D;}
    span.GramE
    	{mso-style-name:"";
    	mso-gram-e:yes;}
    .MsoChpDefault
    	{mso-style-type:export-only;
    	mso-default-props:yes;
    	font-size:10.0pt;
    	mso-ansi-font-size:10.0pt;
    	mso-bidi-font-size:10.0pt;}
    @page WordSection1
    	{size:8.5in 11.0in;
    	margin:1.0in 1.0in 1.0in 1.0in;
    	mso-header-margin:.5in;
    	mso-footer-margin:.5in;
    	mso-paper-source:0;}
    div.WordSection1
    	{page:WordSection1;}
     /* List Definitions */
     @list l0
    	{mso-list-id:159584610;
    	mso-list-template-ids:1034472576;}
    @list l0:level1
    	{mso-level-number-format:bullet;
    	mso-level-text:\F0B7;
    	mso-level-tab-stop:.5in;
    	mso-level-number-position:left;
    	text-indent:-.25in;
    	mso-ansi-font-size:10.0pt;
    	font-family:Symbol;}
    @list l0:level2
    	{mso-level-number-format:bullet;
    	mso-level-text:o;
    	mso-level-tab-stop:1.0in;
    	mso-level-number-position:left;
    	text-indent:-.25in;
    	mso-ansi-font-size:10.0pt;
    	font-family:"Courier New";
    	mso-bidi-font-family:"Times New Roman";}
    @list l0:level3
    	{mso-level-number-format:bullet;
    	mso-level-text:\F0A7;
    	mso-level-tab-stop:1.5in;
    	mso-level-number-position:left;
    	text-indent:-.25in;
    	mso-ansi-font-size:10.0pt;
    	font-family:Wingdings;}
    @list l0:level4
    	{mso-level-number-format:bullet;
    	mso-level-text:\F0A7;
    	mso-level-tab-stop:2.0in;
    	mso-level-number-position:left;
    	text-indent:-.25in;
    	mso-ansi-font-size:10.0pt;
    	font-family:Wingdings;}
    @list l0:level5
    	{mso-level-number-format:bullet;
    	mso-level-text:\F0A7;
    	mso-level-tab-stop:2.5in;
    	mso-level-number-position:left;
    	text-indent:-.25in;
    	mso-ansi-font-size:10.0pt;
    	font-family:Wingdings;}
    @list l0:level6
    	{mso-level-number-format:bullet;
    	mso-level-text:\F0A7;
    	mso-level-tab-stop:3.0in;
    	mso-level-number-position:left;
    	text-indent:-.25in;
    	mso-ansi-font-size:10.0pt;
    	font-family:Wingdings;}
    @list l0:level7
    	{mso-level-number-format:bullet;
    	mso-level-text:\F0A7;
    	mso-level-tab-stop:3.5in;
    	mso-level-number-position:left;
    	text-indent:-.25in;
    	mso-ansi-font-size:10.0pt;
    	font-family:Wingdings;}
    @list l0:level8
    	{mso-level-number-format:bullet;
    	mso-level-text:\F0A7;
    	mso-level-tab-stop:4.0in;
    	mso-level-number-position:left;
    	text-indent:-.25in;
    	mso-ansi-font-size:10.0pt;
    	font-family:Wingdings;}
    @list l0:level9
    	{mso-level-number-format:bullet;
    	mso-level-text:\F0A7;
    	mso-level-tab-stop:4.5in;
    	mso-level-number-position:left;
    	text-indent:-.25in;
    	mso-ansi-font-size:10.0pt;
    	font-family:Wingdings;}
    @list l1
    	{mso-list-id:1778141152;
    	mso-list-template-ids:1534093858;}
    @list l1:level1
    	{mso-level-number-format:bullet;
    	mso-level-text:\F0B7;
    	mso-level-tab-stop:.5in;
    	mso-level-number-position:left;
    	text-indent:-.25in;
    	mso-ansi-font-size:10.0pt;
    	font-family:Symbol;}
    ol
    	{margin-bottom:0in;}
    ul
    	{margin-bottom:0in;}
    -->
    </style>
    <!--[if gte mso 10]>
    <style>
     /* Style Definitions */
     table.MsoNormalTable
    	{mso-style-name:"Table Normal";
    	mso-tstyle-rowband-size:0;
    	mso-tstyle-colband-size:0;
    	mso-style-noshow:yes;
    	mso-style-priority:99;
    	mso-style-qformat:yes;
    	mso-style-parent:"";
    	mso-padding-alt:0in 5.4pt 0in 5.4pt;
    	mso-para-margin:0in;
    	mso-para-margin-bottom:.0001pt;
    	mso-pagination:widow-orphan;
    	font-size:10.0pt;
    	font-family:"Times New Roman","serif";}
    </style>
    <![endif]--><!--[if gte mso 9]><xml>
     <o:shapedefaults v:ext="edit" spidmax="2050"/>
    </xml><![endif]--><!--[if gte mso 9]><xml>
     <o:shapelayout v:ext="edit">
      <o:idmap v:ext="edit" data="1"/>
     </o:shapelayout></xml><![endif]-->
    </head>
    
    <body lang=EN-US link=blue vlink=purple style='tab-interval:.5in'>
    
    <div class=WordSection1>
    
    <p class=MsoNormal><span style='font-size:11.0pt;font-family:"Calibri","sans-serif";
    color:#1F497D'><o:p>&nbsp;</o:p></span></p>
    
    <p class=MsoNormal><span style='font-size:11.0pt;font-family:"Cambria","serif";
    color:#1F497D'>Hello Jody, <o:p></o:p></span></p>
    
    <p class=MsoNormal><span style='font-size:11.0pt;font-family:"Cambria","serif";
    color:#1F497D'>I was speaking with Steven today and he clarified to me the
    &quot;issue&quot; they have faced with the Bluetooth signal.<o:p></o:p></span></p>
    
    <p class=MsoNormal><span style='font-size:11.0pt;font-family:"Cambria","serif";
    color:#1F497D'><o:p>&nbsp;</o:p></span></p>
    
    <p class=MsoNormal><span style='font-size:11.0pt;font-family:"Cambria","serif";
    color:#1F497D'>The performance of the BT signal is not the expected, due to
    different cycles of the signal. The expected performance would be a signal with
    cycles of &quot;power-on&quot; and &quot;power-off&quot; with a constant
    period/behavior.<o:p></o:p></span></p>
    
    <p class=MsoNormal><span style='font-size:11.0pt;color:#1F497D'><o:p>&nbsp;</o:p></span></p>
    
    <p class=MsoNormal><span style='mso-fareast-language:EN-US;mso-no-proof:yes'><!--[if gte vml 1]><v:shapetype
     id="_x0000_t75" coordsize="21600,21600" o:spt="75" o:preferrelative="t"
     path="m@4@5l@4@11@9@11@9@5xe" filled="f" stroked="f">
     <v:stroke joinstyle="miter"/>
     <v:formulas>
      <v:f eqn="if lineDrawn pixelLineWidth 0"/>
      <v:f eqn="sum @0 1 0"/>
      <v:f eqn="sum 0 0 @1"/>
      <v:f eqn="prod @2 1 2"/>
      <v:f eqn="prod @3 21600 pixelWidth"/>
      <v:f eqn="prod @3 21600 pixelHeight"/>
      <v:f eqn="sum @0 0 1"/>
      <v:f eqn="prod @6 1 2"/>
      <v:f eqn="prod @7 21600 pixelWidth"/>
      <v:f eqn="sum @8 21600 0"/>
      <v:f eqn="prod @7 21600 pixelHeight"/>
      <v:f eqn="sum @10 21600 0"/>
     </v:formulas>
     <v:path o:extrusionok="f" gradientshapeok="t" o:connecttype="rect"/>
     <o:lock v:ext="edit" aspectratio="t"/>
    </v:shapetype><v:shape id="Picture_x0020_1" o:spid="_x0000_i1030" type="#_x0000_t75"
     alt="cid:image015.jpg@01CE052E.01132730" style='width:206.4pt;height:180pt;
     visibility:visible;mso-wrap-style:square'>
     <v:imagedata src="Bluetooth%20link%20issue_files/image001.jpg" o:title="image015.jpg@01CE052E"/>
    </v:shape><![endif]--><![if !vml]><img width=275 height=240
    src="Bluetooth%20link%20issue_files/image001.jpg"
    alt="cid:image015.jpg@01CE052E.01132730" v:shapes="Picture_x0020_1"><![endif]></span><span
    style='font-size:11.0pt;font-family:"Cambria","serif";color:#1F497D'><o:p></o:p></span></p>
    
    <p class=MsoNormal><span style='font-size:11.0pt;font-family:"Cambria","serif";
    color:#1F497D'><o:p>&nbsp;</o:p></span></p>
    
    <p class=MsoNormal><span style='font-size:11.0pt;font-family:"Cambria","serif";
    color:#1F497D'>But they are receiving from your device a BT signal that is not
    consistent, the &quot;power-on&quot; cycles are not the expected:<o:p></o:p></span></p>
    
    <p class=MsoNormal><span style='font-size:11.0pt;font-family:"Cambria","serif";
    color:#1F497D'><o:p>&nbsp;</o:p></span></p>
    
    <p class=MsoNormal><span style='mso-fareast-language:EN-US;mso-no-proof:yes'><!--[if gte vml 1]><v:shape
     id="Picture__x000d__x000a__x0020_x0020_2" o:spid="_x0000_i1029" type="#_x0000_t75"
     alt="cid:image016.jpg@01CE052E.01132730" style='width:324pt;height:179.4pt;
     visibility:visible;mso-wrap-style:square'>
     <v:imagedata src="Bluetooth%20link%20issue_files/image002.jpg" o:title="image016.jpg@01CE052E"/>
    </v:shape><![endif]--><![if !vml]><img width=432 height=239
    src="Bluetooth%20link%20issue_files/image002.jpg"
    alt="cid:image016.jpg@01CE052E.01132730" v:shapes="Picture__x000d__x000a__x0020_x0020_2"><![endif]></span><span
    style='font-size:11.0pt;font-family:"Cambria","serif";color:#1F497D'><o:p></o:p></span></p>
    
    <p class=MsoNormal><span style='font-size:11.0pt;font-family:"Cambria","serif";
    color:#1F497D'><o:p>&nbsp;</o:p></span></p>
    
    <p class=MsoNormal><span style='font-size:11.0pt;font-family:"Cambria","serif";
    color:#1F497D'>We need a confirmation from your side that the Bluetooth signal
    behavior shown here is the expected and is correct. In other case, we would
    need next steps to stabilize the signal.<o:p></o:p></span></p>
    
    <p class=MsoNormal><span style='font-size:11.0pt;font-family:"Cambria","serif";
    color:#1F497D'><o:p>&nbsp;</o:p></span></p>
    
    <p class=MsoNormal><span style='font-size:11.0pt;font-family:"Cambria","serif";
    color:#1F497D'>Thanks and regards,<o:p></o:p></span></p>
    
    <p class=MsoNormal><span style='font-size:11.0pt;font-family:"Cambria","serif";
    color:#1F497D'>Ignacio<o:p></o:p></span></p>
    
    <p class=MsoNormal><o:p>&nbsp;</o:p></p>
    
    <p class=MsoNormal><o:p>&nbsp;</o:p></p>
    
    <p class=MsoNormal><o:p>&nbsp;</o:p></p>
    
    <p class=MsoNormal><span style='font-size:10.0pt;font-family:"Arial","sans-serif"'>Hi
    Nacho</span> <br>
    <span style='font-size:10.0pt;font-family:"Arial","sans-serif"'>&nbsp;
    &nbsp;For BT part </span><br>
    <span style='font-size:10.0pt;font-family:"Arial","sans-serif"'>we want to perform
    Dwell time as below describe </span><br>
    <span style='font-size:10.0pt;font-family:"Arial","sans-serif"'>I also attach
    the normal picture as below as red part </span><br>
    <span style='font-size:10.0pt;font-family:"Arial \, sans-serif"'>The red circle
    is mean power on and it is really regular </span><br>
    <br>
    <span style='font-size:10.0pt;font-family:"Arial","sans-serif"'>but <span
    class=GramE>the &nbsp;wave</span> figure is not regular as green circle of your
    product </span><br>
    <span style='font-size:10.0pt;font-family:"Arial","sans-serif"'>so this the
    reason I should confirm for you </span><br>
    <span style='font-size:10.0pt;font-family:"Arial","sans-serif"'>Please let me
    know if you have any concern </span><br>
    <br>
    <br>
    <span style='mso-fareast-language:EN-US;mso-no-proof:yes'><!--[if gte vml 1]><v:shape
     id="Picture_x0020_3" o:spid="_x0000_i1028" type="#_x0000_t75" alt="cid:image001.gif@01CE051A.28166D10"
     style='width:593.4pt;height:120pt;visibility:visible;mso-wrap-style:square'>
     <v:imagedata src="Bluetooth%20link%20issue_files/image003.gif" o:title="image001.gif@01CE051A"/>
    </v:shape><![endif]--><![if !vml]><img width=791 height=160
    src="Bluetooth%20link%20issue_files/image003.gif"
    alt="cid:image001.gif@01CE051A.28166D10" v:shapes="Picture_x0020_3"><![endif]></span><br>
    <span style='mso-fareast-language:EN-US;mso-no-proof:yes'><!--[if gte vml 1]><v:shape
     id="Picture_x0020_4" o:spid="_x0000_i1027" type="#_x0000_t75" alt="cid:image002.gif@01CE051A.28166D10"
     style='width:495pt;height:259.8pt;visibility:visible;mso-wrap-style:square'>
     <v:imagedata src="Bluetooth%20link%20issue_files/image004.gif" o:title="image002.gif@01CE051A"/>
    </v:shape><![endif]--><![if !vml]><img width=660 height=346
    src="Bluetooth%20link%20issue_files/image004.gif"
    alt="cid:image002.gif@01CE051A.28166D10" v:shapes="Picture_x0020_4"><![endif]></span><br>
    <span style='mso-fareast-language:EN-US;mso-no-proof:yes'><!--[if gte vml 1]><v:shape
     id="Picture_x0020_5" o:spid="_x0000_i1026" type="#_x0000_t75" alt="cid:image003.gif@01CE051A.28166D10"
     style='width:500.4pt;height:255pt;visibility:visible;mso-wrap-style:square'>
     <v:imagedata src="Bluetooth%20link%20issue_files/image005.gif" o:title="image003.gif@01CE051A"/>
    </v:shape><![endif]--><![if !vml]><img width=667 height=340
    src="Bluetooth%20link%20issue_files/image005.gif"
    alt="cid:image003.gif@01CE051A.28166D10" v:shapes="Picture_x0020_5"><![endif]></span><br>
    <b><span style='font-size:10.0pt;font-family:"Arial","sans-serif"'>Normal
    figure </span></b><br>
    <br>
    <span style='mso-fareast-language:EN-US;mso-no-proof:yes'><!--[if gte vml 1]><v:shape
     id="Picture_x0020_6" o:spid="_x0000_i1025" type="#_x0000_t75" alt="cid:image004.gif@01CE051A.28166D10"
     style='width:597pt;height:221.4pt;visibility:visible;mso-wrap-style:square'>
     <v:imagedata src="Bluetooth%20link%20issue_files/image006.gif" o:title="image004.gif@01CE051A"/>
    </v:shape><![endif]--><![if !vml]><img width=796 height=295
    src="Bluetooth%20link%20issue_files/image006.gif"
    alt="cid:image004.gif@01CE051A.28166D10" v:shapes="Picture_x0020_6"><![endif]></span><br>
    <br style='mso-special-character:line-break'>
    <![if !supportLineBreakNewLine]><br style='mso-special-character:line-break'>
    <![endif]><s><span style='font-size:10.0pt;font-family:"Arial","sans-serif"'><o:p></o:p></span></s></p>
    
    </div>
    
    </body>
    
    </html>
    

     

    attached is some Bluetooth test the FCC lab is performing.   Do you have any comments regarding their questions

     

    Thanks

  • does TI have any comments or feedback on this ??

  • I assume the question is really regarding placing the Bluetooth subsystem into a mode for continuous transmit, etc.

    The following wiki article describes the procedure.

    http://processors.wiki.ti.com/index.php/Bluetooth_FCC_Mode#WL1271_.2B_ARM_Platforms

     

  • kh123 said:

    We are currently preparing production using Murata Wifi/BT module and we would like to know if we need to do calibration on every module in our production process ??

    Yes, calibration is needed on each module device.

     

    kh123 said:

    it is require to run nvs calibration for every individual unit that we ship?  And is this to tweak power settings so that the units are more consistent in their Tx power and Rx sensitivity?  So if calibration were not performed on each unit, some units would have potentially lower wifi performance?

    Yes, this is likely.

    kh123 said:

    if we are require to perform calibration on every unit, then does a wifi external antenna need to be attached during calibration?  Or is it something internal in the chip?

    I suspect this would be dependent on the module itself.

     

    http://linuxwireless.org/en/users/Drivers/wl12xx/calibrator#wl12xx_Calibration

     

  • the FCC lab already have all these information.

    2543.Bluetooth link issue.doc

    see attached BT link issue posted by the FCC lab.   what the lab want to know is what is the exact linux command syntax in order to make Murata BT module to show the same standard BT signal output