I am using the CC3200 SPI Peripheral and need to create a SPI Clock that does not have a gap between each word.
The Clock currently looks like the below image (noticed the extra clock cycle between each 8 bit word)
I need Clock to look like this (Notice no extra clock cycle between each 8 bit word)
I have tried many settings but still cannot get it to be continuous. I was able to make this continuous when developing on the Tiva C LaunchPad, but all I did on this was set the Phase to 1 and the Polarity to 1. This does not seem to be the case with the CC3200.
Any suggestions are greatly appreciated!
Glenn.