This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

About Wl1271 module bluetooth hardware code 0x06

Other Parts Discussed in Thread: WL1271

Hi All,

Our platform is software: wilink6 + Wince compact 2013 and hardware:  wl1271.

In the process of  running script ( which is implemented in function RunScript() in file bthci.cpp and the script file is brf61_7.6.15.bts),  wl1271 send a event to host.  I print out the event context as below:

        04 10 01 06

Refer to Bluetooth specification,  0x04 means it is a event packet. 0x10 means Hardware Error ocurred in the wl1271 module. 0x01 means parameter length is 1 and 0x06 is the hardware codes.

       I do not know what does the hardware code 0x06 mean? Could you give me a hint on this topic or correct me if I am wrong.

       Thank you!