Dear Experts
My customer plans to use CC3200 with TRF7970 for their smart lock application.
Currently they finished almost all the f/w porting on CC3200 but got issue when porting MIFARE DESFire tag AES-128 encryption (NFC Type 4A tag).
We do provide example code and library AES_Encryption.lib on MSP430G2 but this lib cannot work on CC3200.
May I used the hardware encryption engine on CC3200 for MIFARE DESFire tag AES-128?
Is there any example code to implement this function on CC3200?
Thanks for your comment.