Other Parts Discussed in Thread: BOOSTXL-K350QVG-S1, CC3220SF
Hi,
I am working on a project where I need to have two separate microcontrollers communicating wirelessly, they do not have to be the same. The first microcontroller will be connected to JPEG camera and it will take pictures, at highest speed possible, and send them wirelessly to the second microcontroller. The second microcontroller will be connected to touchscreen and it will project received images onto the screen. I was planning to use CC3200 chips for my project, but I was wondering if they are the best solution for my project. I need microcontroller with substantial RAM (256 kB) and flash (512 kB) so that it can store JPEG picture internally.
My questions are:
1. Are CC3200s the best chips for my application, since they have on-chip wifi and I can use that as my RF link?
2. Can BOOSTXL-K350QVG-S1 Kentec QVGA Display BoosterPack be used with CC3200. I read that it is not compatible with CC3200 Launchpad, but does that mean that is incompatible with the chip as well?
3. Do you still sell CC3200 Camera Booster Pack?
4. What is the indoor and outdoor range that CC3200s can support among themselves?
Thank you