Hello Guys,
The thing is i have a book named as DSP with TIVA, in which the author mention's the use of TIVA Tm4c123G Launchpad with Circuitco Booster Pack to perform some DSP related Processing(Audio Filtering,IIR,FIR etc).
& i guess that booster pack is not anymore available online.So i was wondering to do same with CC3200 WIFI Launchpad & CC3200 Audio Booster but here the thing is i want to do it with simple library functions using TIVAWARE API's.
As CC3200 launchpad uses Simplink Wifi Libraries for event handlers,API's & Protocols to initialize the processor but i donot want to use WIFI handlers for my process.
So is it possible to just use TIVAWARE API's to run some DSP Algorithmns on CC3200 LAunchpadPlus CC3200 audio Booster.
Regards
Sajad