Other Parts Discussed in Thread: , CC3200AUDBOOST, CC1310, CC256XSTBTBLESW
I am trying to get the CC2564 to function with a head set. I have the MSP-EXP432P401R and a BOOST-CC2564MODA set of cards. I only have one set. However, I am trying to use the CC256X TI Bluetooth Stack HSPDemp app to communicate with the head set.
In the HSP Demo it has an Example: Audio gateway with a commercial headset. I have get to the point where the procedure says to Respond with the command: PINCodeResponse. I input PINCodeResponse 0000 and it comes back with an error. If I put in Pair I get further, but it ends up with an error. Is there any step by step procedure about how to get the CC2564 to work with a headset?
Our application is to have a blue tooth headset or just a blue tooth microphone and a CC2564 as the receiver. The CC2564 needs to receive the voice from the microphone and output I2S data. That I2S is summed together in hardware to add a tone from a Metronome. The data is then transmitted via at CC1312 at 900mhz to a remote received.