Other Parts Discussed in Thread: CC3220SF, UNIFLASH, CC3200, TPS62163, TPS62162
Tool/software: Code Composer Studio
Hai,
have a custom designed PCB based on the CC3220SF and i can not communicate uniflash and Debug
We have not been able to flash our code even once and have not been able to connect it using uniflash to change from production to development mode.
i followed www.ti.com/.../swru462 (Design Checklist) ... all are fine
share my Schematic connection
1.DCDC -ANA2-SW-P ---> 0v
2.DCDC- ANA2-SW-N ---> 0v
3.VDD- ANA2 ----> 0v
but voltage ref (1.6V)
the actual voltage is 1.6 but we are getting 0v
any other change in schematic or resistance value
TI Schematic File Snapshot
TI_Board voltage across is fine ( 1.6V) ..
(Design Checklist)---> Followed component is use to pcb board
this components BOM part Number will be used ..
how to solve this issue ..?????
Following Testing voltage Mesurement
Test Point TI Board || My Own Board
VIN_IO1 -> 3.3V 3.3V
VIN_IO2 -> 3.3V 3.3V
VIN_DCDC_DIG -> 3.3V 3.3V
VIN_DCDC_PA -> 3.3V 3.3V
VIN_DCDC_ANA -> 3.3V 3.3V
DCDC_ANA_SW -> 1.9V 1.9V
VDD_ANA1 -> 1.9V 1.9V
LDO_IN1 -> 1.9V 1.9V
LDO_IN2 -> 1.9V 1.9V
DCDC_PA_OUT -> 0V 0V
VDD_PA_IN -> 0V 0V
DCDC_DIG_SW -> 1.2V 1.2V
VDD_DIG1 -> 1.2V 1.2V
VDD_DIG2 -> 1.2V 1.2V
DCDC_ANA2_SW_P -> 1.6V 0V ( issue point)
DCDC_ANA2_SW_N -> 1.6V 0V ( issue point)
VDD_ANA2 -> 3.2V 0V ( issue point)
VDD_RAN -> 1.2V 1.2V
VDD_PLL -> 0V 0V
Any other solution at this issue--> how to power up the board , uniflash also not connect..
Thanks
SELVA