This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CCS/CC3220SF-LAUNCHXL: The differences between UART_write and UART_print when the UART routed to 20-Pin header connector

Part Number: CC3220SF-LAUNCHXL

Tool/software: Code Composer Studio

Now,I configure my jumpers to be placed as shown in Figure 14 ,will the UART_print statement in the example write the strings(which are sent to the USB Teminal) into the UART pin and give them to other boards? Should I annotation them?