Other Parts Discussed in Thread: WL1271
Hi Guys,
I am seeing exactly the same error as the related post.
Everything works for us normally, however over time we get the kernel module crash maybe after a few hours often after a few days of being connected to an access point.
We have tried various versions of the firmware and currently are using the latest to see if the problem is fixed, but it still persists.
wlcore: wl18xx HW: 183x or 180x, PG 2.2 (ROM 0x11)
wlcore: PHY firmware version: Rev 8.2.0.0.245
wlcore: firmware booted (Rev 8.9.0.0.86)
We have used kernel 4.9.220-fslc and 4.9.253-fslc (latest 4.9) and the problem still exists.
Currently we are running tests on beta sites with ELP disabled to see if we can narrow down the problem to this functionality. We are waiting on the results.
This is a summary of the trace we are seeing:
Jan 30 13:58:56 testdevice kernel: WARNING: CPU: 1 PID: 2603 at /usr/src/kernel/drivers/net/wireless/ti/wlcore/sdio.c:145 wl12xx_sdio_raw_write+0xec/0x1c8 [wlcore_sdio] Jan 30 13:58:56 testdevice kernel: Modules linked in: wl18xx wlcore mac80211 wlcore_sdio galcore(O) cfg80211 Jan 30 13:58:56 testdevice kernel: CPU: 1 PID: 2603 Comm: kworker/u4:1 Tainted: G O 4.9.253-fslc+g4faee40 #1 Jan 30 13:58:56 testdevice kernel: Hardware name: Freescale i.MX6 Quad/DualLite (Device Tree) Jan 30 13:58:56 testdevice kernel: Workqueue: phy0 wl1271_tx_work [wlcore] Jan 30 13:58:56 testdevice kernel: Backtrace: Jan 30 13:58:56 testdevice kernel: [<8010ca54>] (dump_backtrace) from [<8010cd48>] (show_stack+0x18/0x1c) Jan 30 13:58:56 testdevice kernel: r7:60030113 r6:80e200b0 r5:00000000 r4:80e200b0 Jan 30 13:58:56 testdevice kernel: [<8010cd30>] (show_stack) from [<80963718>] (dump_stack+0x8c/0xa0) Jan 30 13:58:56 testdevice kernel: [<8096368c>] (dump_stack) from [<80127c98>] (__warn+0xec/0x104) Jan 30 13:58:56 testdevice kernel: r7:00000009 r6:7f12cab8 r5:00000000 r4:00000000 Jan 30 13:58:56 testdevice kernel: [<80127bac>] (__warn) from [<80127db0>] (warn_slowpath_null+0x28/0x30) Jan 30 13:58:56 testdevice kernel: r9:00000004 r8:a86aa200 r7:a879f210 r6:0001fffc r5:80e04148 r4:a847d000 Jan 30 13:58:56 testdevice kernel: [<80127d88>] (warn_slowpath_null) from [<7f12b2f4>] (wl12xx_sdio_raw_write+0xec/0x1c8 [wlcore_sdio]) Jan 30 13:58:56 testdevice kernel: [<7f12b208>] (wl12xx_sdio_raw_write [wlcore_sdio]) from [<7f1bdbb4>] (wl1271_ps_elp_wakeup+0x124/0x258 [wlcore]) Jan 30 13:58:56 testdevice kernel: r10:a9110e04 r9:7f1d3340 r8:00098c70 r7:a9110e34 r6:80e02d00 r5:a9110de0 Jan 30 13:58:56 testdevice kernel: r4:80e04148 Jan 30 13:58:56 testdevice kernel: [<7f1bda90>] (wl1271_ps_elp_wakeup [wlcore]) from [<7f1bcb6c>] (wl1271_tx_work+0x24/0x58 [wlcore]) Jan 30 13:58:56 testdevice kernel: r10:80e02d00 r9:00000000 r8:00000000 r7:a8818200 r6:a8002800 r5:a9110e1c Jan 30 13:58:56 testdevice kernel: r4:a9110de0 Jan 30 13:58:56 testdevice kernel: [<7f1bcb48>] (wl1271_tx_work [wlcore]) from [<80140444>] (process_one_work+0x1dc/0x3f4) Jan 30 13:58:56 testdevice kernel: r5:a919c480 r4:a9110fc0 Jan 30 13:58:56 testdevice kernel: [<80140268>] (process_one_work) from [<80141438>] (worker_thread+0x68/0x5c0) Jan 30 13:58:56 testdevice kernel: r10:80e02d00 r9:00000088 r8:ffffe000 r7:a8002818 r6:a919c498 r5:a8002800 Jan 30 13:58:56 testdevice kernel: r4:a919c480 Jan 30 13:58:56 testdevice kernel: [<801413d0>] (worker_thread) from [<80146a2c>] (kthread+0x120/0x128) Jan 30 13:58:56 testdevice kernel: r10:00000000 r9:00000000 r8:801413d0 r7:a919c480 r6:a91ca000 r5:a91e31c0 Jan 30 13:58:56 testdevice kernel: r4:00000000 Jan 30 13:58:56 testdevice kernel: [<8014690c>] (kthread) from [<80108f30>] (ret_from_fork+0x14/0x24) Jan 30 13:58:56 testdevice kernel: r8:00000000 r7:00000000 r6:00000000 r5:8014690c r4:a91e31c0 Jan 30 13:58:56 testdevice kernel: ---[ end trace 96da51c88605a643 ]--- Jan 30 13:58:56 testdevice kernel: wl1271_sdio mmc0:0001:2: sdio write failed (-110) Jan 30 13:58:56 testdevice kernel: ------------[ cut here ]------------
Does anyone else have any further recommendations as to things to check/test to fix the problem?
We will try reducing the sdio frequency as the next thing to test after the results of ELP disabling come in.
Please let me know if you need
Full stack trace log file attached and wlconf config attached:
header.magic = 0x10e100ca header.version = 0x00070007 header.checksum = 0x00000000 core.sg.params = 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x0000000f, 0x0000001b, 0x00000011, 0x000000aa, 0x00000032, 0x00000064, 0x00000320, 0x000000c8, 0x000000c8, 0x00000000, 0x00000000, 0x00000000, 0x00000001, 0x00000000, 0x0000003c, 0x00001388, 0x000004b0, 0x000003e8, 0x00000001, 0x00000003, 0x00000006, 0x0000000a, 0x0000000a, 0x00000002, 0x00000005, 0x0000001e, 0x00000003, 0x0000000a, 0x00000002, 0x00000000, 0x00000019, 0x00000019, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000, 0x00000000 core.sg.state = 0x01 core.rx.rx_msdu_life_time = 0x0007d000 core.rx.packet_detection_threshold = 0x00000000 core.rx.ps_poll_timeout = 0x000f core.rx.upsd_timeout = 0x000f core.rx.rts_threshold = 0x0931 core.rx.rx_cca_threshold = 0x0000 core.rx.irq_blk_threshold = 0xffff core.rx.irq_pkt_threshold = 0x0000 core.rx.irq_timeout = 0x0258 core.rx.queue_type = 0x00 core.tx.tx_energy_detection = 0x00 core.tx.sta_rc_conf.enabled_rates = 0x00000000 core.tx.sta_rc_conf.short_retry_limit = 0x0a core.tx.sta_rc_conf.long_retry_limit = 0x0a core.tx.sta_rc_conf.aflags = 0x00 core.tx.ac_conf_count = 0x04 core.tx.ac_conf0.ac = 0x00 core.tx.ac_conf0.cw_min = 0x0f core.tx.ac_conf0.cw_max = 0x003f core.tx.ac_conf0.aifsn = 0x03 core.tx.ac_conf0.tx_op_limit = 0x0000 core.tx.ac_conf1.ac = 0x01 core.tx.ac_conf1.cw_min = 0x0f core.tx.ac_conf1.cw_max = 0x003f core.tx.ac_conf1.aifsn = 0x07 core.tx.ac_conf1.tx_op_limit = 0x0000 core.tx.ac_conf2.ac = 0x02 core.tx.ac_conf2.cw_min = 0x0f core.tx.ac_conf2.cw_max = 0x003f core.tx.ac_conf2.aifsn = 0x01 core.tx.ac_conf2.tx_op_limit = 0x0bc0 core.tx.ac_conf3.ac = 0x03 core.tx.ac_conf3.cw_min = 0x0f core.tx.ac_conf3.cw_max = 0x003f core.tx.ac_conf3.aifsn = 0x01 core.tx.ac_conf3.tx_op_limit = 0x05e0 core.tx.max_tx_retries = 0x64 core.tx.ap_aging_period = 0x012c core.tx.tid_conf_count = 0x04 core.tx.tid_conf0.queue_id = 0x00 core.tx.tid_conf0.channel_type = 0x01 core.tx.tid_conf0.tsid = 0x00 core.tx.tid_conf0.ps_scheme = 0x00 core.tx.tid_conf0.ack_policy = 0x00 core.tx.tid_conf0.apsd_conf = 0x00000000, 0x00000000 core.tx.tid_conf1.queue_id = 0x01 core.tx.tid_conf1.channel_type = 0x01 core.tx.tid_conf1.tsid = 0x01 core.tx.tid_conf1.ps_scheme = 0x00 core.tx.tid_conf1.ack_policy = 0x00 core.tx.tid_conf1.apsd_conf = 0x00000000, 0x00000000 core.tx.tid_conf2.queue_id = 0x02 core.tx.tid_conf2.channel_type = 0x01 core.tx.tid_conf2.tsid = 0x02 core.tx.tid_conf2.ps_scheme = 0x00 core.tx.tid_conf2.ack_policy = 0x00 core.tx.tid_conf2.apsd_conf = 0x00000000, 0x00000000 core.tx.tid_conf3.queue_id = 0x03 core.tx.tid_conf3.channel_type = 0x01 core.tx.tid_conf3.tsid = 0x03 core.tx.tid_conf3.ps_scheme = 0x00 core.tx.tid_conf3.ack_policy = 0x00 core.tx.tid_conf3.apsd_conf = 0x00000000, 0x00000000 core.tx.tid_conf4.queue_id = 0x00 core.tx.tid_conf4.channel_type = 0x00 core.tx.tid_conf4.tsid = 0x00 core.tx.tid_conf4.ps_scheme = 0x00 core.tx.tid_conf4.ack_policy = 0x00 core.tx.tid_conf4.apsd_conf = 0x00000000, 0x00000000 core.tx.tid_conf5.queue_id = 0x00 core.tx.tid_conf5.channel_type = 0x00 core.tx.tid_conf5.tsid = 0x00 core.tx.tid_conf5.ps_scheme = 0x00 core.tx.tid_conf5.ack_policy = 0x00 core.tx.tid_conf5.apsd_conf = 0x00000000, 0x00000000 core.tx.tid_conf6.queue_id = 0x00 core.tx.tid_conf6.channel_type = 0x00 core.tx.tid_conf6.tsid = 0x00 core.tx.tid_conf6.ps_scheme = 0x00 core.tx.tid_conf6.ack_policy = 0x00 core.tx.tid_conf6.apsd_conf = 0x00000000, 0x00000000 core.tx.tid_conf7.queue_id = 0x00 core.tx.tid_conf7.channel_type = 0x00 core.tx.tid_conf7.tsid = 0x00 core.tx.tid_conf7.ps_scheme = 0x00 core.tx.tid_conf7.ack_policy = 0x00 core.tx.tid_conf7.apsd_conf = 0x00000000, 0x00000000 core.tx.frag_threshold = 0x0930 core.tx.tx_compl_timeout = 0x015e core.tx.tx_compl_threshold = 0x000a core.tx.basic_rate = 0x00000001 core.tx.basic_rate_5 = 0x00000008 core.tx.tmpl_short_retry_limit = 0x0a core.tx.tmpl_long_retry_limit = 0x0a core.tx.tx_watchdog_timeout = 0x00001388 core.tx.slow_link_thold = 0x03 core.tx.fast_link_thold = 0x1e core.conn.wake_up_event = 0x02 core.conn.listen_interval = 0x01 core.conn.suspend_wake_up_event = 0x04 core.conn.suspend_listen_interval = 0x03 core.conn.bcn_filt_mode = 0x01 core.conn.bcn_filt_ie_count = 0x03 core.conn.bcn_filt_ie0.ie = 0x25 core.conn.bcn_filt_ie0.rule = 0x02 core.conn.bcn_filt_ie0.oui = 0x00, 0x00, 0x00 core.conn.bcn_filt_ie0.type = 0x00 core.conn.bcn_filt_ie0.version = 0x00, 0x00 core.conn.bcn_filt_ie1.ie = 0x3d core.conn.bcn_filt_ie1.rule = 0x01 core.conn.bcn_filt_ie1.oui = 0x00, 0x00, 0x00 core.conn.bcn_filt_ie1.type = 0x00 core.conn.bcn_filt_ie1.version = 0x00, 0x00 core.conn.bcn_filt_ie2.ie = 0x2a core.conn.bcn_filt_ie2.rule = 0x01 core.conn.bcn_filt_ie2.oui = 0x00, 0x00, 0x00 core.conn.bcn_filt_ie2.type = 0x00 core.conn.bcn_filt_ie2.version = 0x00, 0x00 core.conn.bcn_filt_ie3.ie = 0x00 core.conn.bcn_filt_ie3.rule = 0x00 core.conn.bcn_filt_ie3.oui = 0x00, 0x00, 0x00 core.conn.bcn_filt_ie3.type = 0x00 core.conn.bcn_filt_ie3.version = 0x00, 0x00 core.conn.bcn_filt_ie4.ie = 0x00 core.conn.bcn_filt_ie4.rule = 0x00 core.conn.bcn_filt_ie4.oui = 0x00, 0x00, 0x00 core.conn.bcn_filt_ie4.type = 0x00 core.conn.bcn_filt_ie4.version = 0x00, 0x00 core.conn.bcn_filt_ie5.ie = 0x00 core.conn.bcn_filt_ie5.rule = 0x00 core.conn.bcn_filt_ie5.oui = 0x00, 0x00, 0x00 core.conn.bcn_filt_ie5.type = 0x00 core.conn.bcn_filt_ie5.version = 0x00, 0x00 core.conn.bcn_filt_ie6.ie = 0x00 core.conn.bcn_filt_ie6.rule = 0x00 core.conn.bcn_filt_ie6.oui = 0x00, 0x00, 0x00 core.conn.bcn_filt_ie6.type = 0x00 core.conn.bcn_filt_ie6.version = 0x00, 0x00 core.conn.bcn_filt_ie7.ie = 0x00 core.conn.bcn_filt_ie7.rule = 0x00 core.conn.bcn_filt_ie7.oui = 0x00, 0x00, 0x00 core.conn.bcn_filt_ie7.type = 0x00 core.conn.bcn_filt_ie7.version = 0x00, 0x00 core.conn.bcn_filt_ie8.ie = 0x00 core.conn.bcn_filt_ie8.rule = 0x00 core.conn.bcn_filt_ie8.oui = 0x00, 0x00, 0x00 core.conn.bcn_filt_ie8.type = 0x00 core.conn.bcn_filt_ie8.version = 0x00, 0x00 core.conn.bcn_filt_ie9.ie = 0x00 core.conn.bcn_filt_ie9.rule = 0x00 core.conn.bcn_filt_ie9.oui = 0x00, 0x00, 0x00 core.conn.bcn_filt_ie9.type = 0x00 core.conn.bcn_filt_ie9.version = 0x00, 0x00 core.conn.bcn_filt_ie10.ie = 0x00 core.conn.bcn_filt_ie10.rule = 0x00 core.conn.bcn_filt_ie10.oui = 0x00, 0x00, 0x00 core.conn.bcn_filt_ie10.type = 0x00 core.conn.bcn_filt_ie10.version = 0x00, 0x00 core.conn.bcn_filt_ie11.ie = 0x00 core.conn.bcn_filt_ie11.rule = 0x00 core.conn.bcn_filt_ie11.oui = 0x00, 0x00, 0x00 core.conn.bcn_filt_ie11.type = 0x00 core.conn.bcn_filt_ie11.version = 0x00, 0x00 core.conn.bcn_filt_ie12.ie = 0x00 core.conn.bcn_filt_ie12.rule = 0x00 core.conn.bcn_filt_ie12.oui = 0x00, 0x00, 0x00 core.conn.bcn_filt_ie12.type = 0x00 core.conn.bcn_filt_ie12.version = 0x00, 0x00 core.conn.bcn_filt_ie13.ie = 0x00 core.conn.bcn_filt_ie13.rule = 0x00 core.conn.bcn_filt_ie13.oui = 0x00, 0x00, 0x00 core.conn.bcn_filt_ie13.type = 0x00 core.conn.bcn_filt_ie13.version = 0x00, 0x00 core.conn.bcn_filt_ie14.ie = 0x00 core.conn.bcn_filt_ie14.rule = 0x00 core.conn.bcn_filt_ie14.oui = 0x00, 0x00, 0x00 core.conn.bcn_filt_ie14.type = 0x00 core.conn.bcn_filt_ie14.version = 0x00, 0x00 core.conn.bcn_filt_ie15.ie = 0x00 core.conn.bcn_filt_ie15.rule = 0x00 core.conn.bcn_filt_ie15.oui = 0x00, 0x00, 0x00 core.conn.bcn_filt_ie15.type = 0x00 core.conn.bcn_filt_ie15.version = 0x00, 0x00 core.conn.bcn_filt_ie16.ie = 0x00 core.conn.bcn_filt_ie16.rule = 0x00 core.conn.bcn_filt_ie16.oui = 0x00, 0x00, 0x00 core.conn.bcn_filt_ie16.type = 0x00 core.conn.bcn_filt_ie16.version = 0x00, 0x00 core.conn.bcn_filt_ie17.ie = 0x00 core.conn.bcn_filt_ie17.rule = 0x00 core.conn.bcn_filt_ie17.oui = 0x00, 0x00, 0x00 core.conn.bcn_filt_ie17.type = 0x00 core.conn.bcn_filt_ie17.version = 0x00, 0x00 core.conn.bcn_filt_ie18.ie = 0x00 core.conn.bcn_filt_ie18.rule = 0x00 core.conn.bcn_filt_ie18.oui = 0x00, 0x00, 0x00 core.conn.bcn_filt_ie18.type = 0x00 core.conn.bcn_filt_ie18.version = 0x00, 0x00 core.conn.bcn_filt_ie19.ie = 0x00 core.conn.bcn_filt_ie19.rule = 0x00 core.conn.bcn_filt_ie19.oui = 0x00, 0x00, 0x00 core.conn.bcn_filt_ie19.type = 0x00 core.conn.bcn_filt_ie19.version = 0x00, 0x00 core.conn.bcn_filt_ie20.ie = 0x00 core.conn.bcn_filt_ie20.rule = 0x00 core.conn.bcn_filt_ie20.oui = 0x00, 0x00, 0x00 core.conn.bcn_filt_ie20.type = 0x00 core.conn.bcn_filt_ie20.version = 0x00, 0x00 core.conn.bcn_filt_ie21.ie = 0x00 core.conn.bcn_filt_ie21.rule = 0x00 core.conn.bcn_filt_ie21.oui = 0x00, 0x00, 0x00 core.conn.bcn_filt_ie21.type = 0x00 core.conn.bcn_filt_ie21.version = 0x00, 0x00 core.conn.bcn_filt_ie22.ie = 0x00 core.conn.bcn_filt_ie22.rule = 0x00 core.conn.bcn_filt_ie22.oui = 0x00, 0x00, 0x00 core.conn.bcn_filt_ie22.type = 0x00 core.conn.bcn_filt_ie22.version = 0x00, 0x00 core.conn.bcn_filt_ie23.ie = 0x00 core.conn.bcn_filt_ie23.rule = 0x00 core.conn.bcn_filt_ie23.oui = 0x00, 0x00, 0x00 core.conn.bcn_filt_ie23.type = 0x00 core.conn.bcn_filt_ie23.version = 0x00, 0x00 core.conn.bcn_filt_ie24.ie = 0x00 core.conn.bcn_filt_ie24.rule = 0x00 core.conn.bcn_filt_ie24.oui = 0x00, 0x00, 0x00 core.conn.bcn_filt_ie24.type = 0x00 core.conn.bcn_filt_ie24.version = 0x00, 0x00 core.conn.bcn_filt_ie25.ie = 0x00 core.conn.bcn_filt_ie25.rule = 0x00 core.conn.bcn_filt_ie25.oui = 0x00, 0x00, 0x00 core.conn.bcn_filt_ie25.type = 0x00 core.conn.bcn_filt_ie25.version = 0x00, 0x00 core.conn.bcn_filt_ie26.ie = 0x00 core.conn.bcn_filt_ie26.rule = 0x00 core.conn.bcn_filt_ie26.oui = 0x00, 0x00, 0x00 core.conn.bcn_filt_ie26.type = 0x00 core.conn.bcn_filt_ie26.version = 0x00, 0x00 core.conn.bcn_filt_ie27.ie = 0x00 core.conn.bcn_filt_ie27.rule = 0x00 core.conn.bcn_filt_ie27.oui = 0x00, 0x00, 0x00 core.conn.bcn_filt_ie27.type = 0x00 core.conn.bcn_filt_ie27.version = 0x00, 0x00 core.conn.bcn_filt_ie28.ie = 0x00 core.conn.bcn_filt_ie28.rule = 0x00 core.conn.bcn_filt_ie28.oui = 0x00, 0x00, 0x00 core.conn.bcn_filt_ie28.type = 0x00 core.conn.bcn_filt_ie28.version = 0x00, 0x00 core.conn.bcn_filt_ie29.ie = 0x00 core.conn.bcn_filt_ie29.rule = 0x00 core.conn.bcn_filt_ie29.oui = 0x00, 0x00, 0x00 core.conn.bcn_filt_ie29.type = 0x00 core.conn.bcn_filt_ie29.version = 0x00, 0x00 core.conn.bcn_filt_ie30.ie = 0x00 core.conn.bcn_filt_ie30.rule = 0x00 core.conn.bcn_filt_ie30.oui = 0x00, 0x00, 0x00 core.conn.bcn_filt_ie30.type = 0x00 core.conn.bcn_filt_ie30.version = 0x00, 0x00 core.conn.bcn_filt_ie31.ie = 0x00 core.conn.bcn_filt_ie31.rule = 0x00 core.conn.bcn_filt_ie31.oui = 0x00, 0x00, 0x00 core.conn.bcn_filt_ie31.type = 0x00 core.conn.bcn_filt_ie31.version = 0x00, 0x00 core.conn.synch_fail_thold = 0x0000000c core.conn.bss_lose_timeout = 0x00000190 core.conn.beacon_rx_timeout = 0x00002710 core.conn.broadcast_timeout = 0x00004e20 core.conn.rx_broadcast_in_ps = 0x01 core.conn.ps_poll_threshold = 0x0a core.conn.sig_weights.rssi_bcn_avg_weight = 0x00 core.conn.sig_weights.rssi_pkt_avg_weight = 0x00 core.conn.sig_weights.snr_bcn_avg_weight = 0x00 core.conn.sig_weights.snr_pkt_avg_weight = 0x00 core.conn.bet_enable = 0x01 core.conn.bet_max_consecutive = 0x32 core.conn.psm_entry_retries = 0x08 core.conn.psm_exit_retries = 0x10 core.conn.psm_entry_nullfunc_retries = 0x03 core.conn.dynamic_ps_timeout = 0x0096 core.conn.forced_ps = 0x00 core.conn.keep_alive_interval = 0x0000d6d8 core.conn.max_listen_interval = 0x14 core.conn.sta_sleep_auth = 0xff core.conn.suspend_rx_ba_activity = 0x00 core.itrim.enable = 0x00 core.itrim.timeout = 0x0000c350 core.pm_config.host_clk_settling_time = 0x00001388 core.pm_config.host_fast_wakeup_support = 0x01 core.roam_trigger.trigger_pacing = 0x0001 core.roam_trigger.avg_weight_rssi_beacon = 0x14 core.roam_trigger.avg_weight_rssi_data = 0x0a core.roam_trigger.avg_weight_snr_beacon = 0x14 core.roam_trigger.avg_weight_snr_data = 0x0a core.scan.min_dwell_time_active = 0x00001d4c core.scan.max_dwell_time_active = 0x00007530 core.scan.min_dwell_time_active_long = 0x000061a8 core.scan.max_dwell_time_active_long = 0x0000c350 core.scan.dwell_time_passive = 0x000186a0 core.scan.dwell_time_dfs = 0x000249f0 core.scan.num_probe_reqs = 0x0002 core.scan.split_scan_timeout = 0x0000c350 core.sched_scan.base_dwell_time = 0x00001d4c core.sched_scan.max_dwell_time_delta = 0x000057e4 core.sched_scan.dwell_time_delta_per_probe = 0x000007d0 core.sched_scan.dwell_time_delta_per_probe_5 = 0x0000015e core.sched_scan.dwell_time_passive = 0x000186a0 core.sched_scan.dwell_time_dfs = 0x000249f0 core.sched_scan.num_probe_reqs = 0x02 core.sched_scan.rssi_threshold = 0xa6 core.sched_scan.snr_threshold = 0x00 core.sched_scan.num_short_intervals = 0x0d core.sched_scan.long_interval = 0x7530 core.ht.rx_ba_win_size = 0x20 core.ht.tx_ba_win_size = 0x40 core.ht.inactivity_timeout = 0x2710 core.ht.tx_ba_tid_bitmap = 0x3f core.mem.num_stations = 0x01 core.mem.ssid_profiles = 0x01 core.mem.rx_block_num = 0x28 core.mem.tx_min_block_num = 0x28 core.mem.dynamic_memory = 0x01 core.mem.min_req_tx_blocks = 0x2d core.mem.min_req_rx_blocks = 0x16 core.mem.tx_min = 0x1b core.fm_coex.enable = 0x01 core.fm_coex.swallow_period = 0x05 core.fm_coex.n_divider_fref_set_1 = 0xff core.fm_coex.n_divider_fref_set_2 = 0x0c core.fm_coex.m_divider_fref_set_1 = 0xffff core.fm_coex.m_divider_fref_set_2 = 0x0094 core.fm_coex.coex_pll_stabilization_time = 0xffffffff core.fm_coex.ldo_stabilization_time = 0xffff core.fm_coex.fm_disturbed_band_margin = 0xff core.fm_coex.swallow_clk_diff = 0xff core.rx_streaming.duration = 0x00000096 core.rx_streaming.queues = 0x01 core.rx_streaming.interval = 0x14 core.rx_streaming.always = 0x00 core.fwlog.mode = 0x00 core.fwlog.mem_blocks = 0x02 core.fwlog.severity = 0x00 core.fwlog.timestamp = 0x00 core.fwlog.output = 0x01 core.fwlog.threshold = 0x00 core.rate.rate_retry_score = 0x7d00 core.rate.per_add = 0x2000 core.rate.per_th1 = 0x0800 core.rate.per_th2 = 0x1000 core.rate.max_per = 0x1fa4 core.rate.inverse_curiosity_factor = 0x05 core.rate.tx_fail_low_th = 0x04 core.rate.tx_fail_high_th = 0x0a core.rate.per_alpha_shift = 0x04 core.rate.per_add_shift = 0x0d core.rate.per_beta1_shift = 0x0a core.rate.per_beta2_shift = 0x08 core.rate.rate_check_up = 0x02 core.rate.rate_check_down = 0x0c core.rate.rate_retry_policy = 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00 core.hangover.recover_time = 0x00000000 core.hangover.hangover_period = 0x14 core.hangover.dynamic_mode = 0x01 core.hangover.early_termination_mode = 0x01 core.hangover.max_period = 0x14 core.hangover.min_period = 0x01 core.hangover.increase_delta = 0x01 core.hangover.decrease_delta = 0x02 core.hangover.quiet_time = 0x04 core.hangover.increase_time = 0x01 core.hangover.window_size = 0x10 core.recovery.bug_on_recovery = 0x00 core.recovery.no_recovery = 0x00 wl18xx.ht.mode = 0x00 wl18xx.phy.phy_standalone = 0x00 wl18xx.phy.spare0 = 0x08 wl18xx.phy.enable_clpc = 0x00 wl18xx.phy.enable_tx_low_pwr_on_siso_rdl = 0x00 wl18xx.phy.auto_detect = 0x00 wl18xx.phy.dedicated_fem = 0x00 wl18xx.phy.low_band_component = 0x02 wl18xx.phy.low_band_component_type = 0x05 wl18xx.phy.high_band_component = 0x01 wl18xx.phy.high_band_component_type = 0x0a wl18xx.phy.number_of_assembled_ant2_4 = 0x02 wl18xx.phy.number_of_assembled_ant5 = 0x02 wl18xx.phy.pin_muxing_platform_options = 0x00, 0x00 wl18xx.phy.external_pa_dc2dc = 0x00 wl18xx.phy.tcxo_ldo_voltage = 0x00 wl18xx.phy.xtal_itrim_val = 0x04 wl18xx.phy.srf_state = 0x00 wl18xx.phy.srf1 = 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00 wl18xx.phy.srf2 = 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00 wl18xx.phy.srf3 = 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00 wl18xx.phy.io_configuration = 0x01 wl18xx.phy.sdio_configuration = 0x00 wl18xx.phy.settings = 0x00 wl18xx.phy.rx_profile = 0x00 wl18xx.phy.per_chan_pwr_limit_arr_11abg = 0x78, 0x88, 0x88, 0x78, 0x88, 0x88, 0x78, 0x88, 0x88, 0x78, 0x88, 0x88, 0x78, 0x88, 0x18, 0x78, 0x88, 0x88, 0x78, 0x88, 0x82, 0x78, 0x88, 0x88, 0x78, 0x88, 0x88, 0x78, 0x88, 0x88, 0x78, 0x88, 0x88, 0x78, 0x88, 0x88, 0x78, 0x88, 0x88, 0xff, 0xff, 0xff, 0xf8, 0xff, 0xff, 0xf8, 0xff, 0xff, 0xf8, 0xff, 0xff, 0xf8, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xf7, 0x22, 0x22, 0xff, 0xff, 0xff, 0xf7, 0x22, 0x22, 0xff, 0xff, 0xff, 0xf7, 0x66, 0x66, 0xff, 0xff, 0xff, 0xf7, 0x66, 0x66, 0xf4, 0x44, 0x55, 0xf4, 0x44, 0x55, 0xf4, 0x22, 0x22, 0xf4, 0x22, 0x22, 0xf6, 0x44, 0x44, 0xff, 0x44, 0x44, 0xf7, 0x66, 0x66, 0xf7, 0x66, 0x66, 0xf7, 0x66, 0x66, 0xf7, 0x66, 0x66, 0xf7, 0x66, 0x66, 0xf7, 0x66, 0x66, 0xf7, 0x66, 0x55, 0xf7, 0x44, 0x55, 0xf4, 0xff, 0xff, 0xff, 0x33, 0x22, 0xff, 0x33, 0x22, 0xff, 0x66, 0x66, 0xff, 0x44, 0x66, 0xf6, 0xff, 0xff, 0xff, 0xff, 0xff wl18xx.phy.pwr_limit_reference_11_abg = 0x55 wl18xx.phy.per_chan_pwr_limit_arr_11p = 0xff, 0xff, 0xff, 0xff, 0xff, 0xff, 0xff wl18xx.phy.pwr_limit_reference_11p = 0x64 wl18xx.phy.spare1 = 0x00 wl18xx.phy.per_chan_bo_mode_11_abg = 0x40, 0x00, 0x04, 0x30, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x40, 0x19 wl18xx.phy.per_chan_bo_mode_11_p = 0x00, 0x00, 0x00, 0x01 wl18xx.phy.primary_clock_setting_time = 0x05 wl18xx.phy.clock_valid_on_wake_up = 0x00 wl18xx.phy.secondary_clock_setting_time = 0x05 wl18xx.phy.board_type = 0x02 wl18xx.phy.psat = 0x00 wl18xx.phy.low_power_val = 0xff wl18xx.phy.med_power_val = 0xff wl18xx.phy.high_power_val = 0xff wl18xx.phy.per_sub_band_tx_trace_loss = 0x08, 0x18, 0x10, 0x10, 0x10, 0x10, 0x10, 0x10, 0x10, 0x10 wl18xx.phy.per_sub_band_rx_trace_loss = 0x08, 0x18, 0x10, 0x10, 0x10, 0x10, 0x10, 0x10, 0x10, 0x10, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00 wl18xx.phy.tx_rf_margin = 0x01 wl18xx.phy.low_power_val_2nd = 0xff wl18xx.phy.med_power_val_2nd = 0xff wl18xx.phy.high_power_val_2nd = 0xff wl18xx.phy.padding = 0x00 wl18xx.ap_sleep.idle_duty_cycle = 0x00 wl18xx.ap_sleep.connected_duty_cycle = 0x00 wl18xx.ap_sleep.max_stations_thresh = 0x04 wl18xx.ap_sleep.idle_conn_thresh = 0x08