Hi Teams!
I want to built a wireless communication system with requirements as follows.
・Application: to transmit sin/cos signals, between a motor resolver and a control board
・Transmission singals: sin/10V/10kHz, sin/10V/10kHz, sin/10V/10kHz, total 3 signals
The above signals are similar to the singals as drawn in the Figure 2 in the following site.
The black sin signal is transmitted from a control board to a motor resolver, to excite magnetic flux in coil R1-R2 of the motor resolver, as shown in Figure 1.
The blue and red sin/cos signals are transmitted from the motor resolver to the control board, which are excited in coils S1-S3 and S2-S4, as shown in Figure 1.
I haven't ever built a wireless communication system. My questions are as follows.
1)Is there any wireless communication module to transmit the above sin/cos singals?
All the transmission methods are OK, such as ZigBee, Bluetooth, WiFi, etc.
2)If there aren't wireless communication modules to transmit the above signals, could you please tell me how to built a wireless communication system to achive the above purpose?
For excample, I'm considering the following system. Could you please tell me that if it is possible or not, and what chips can be used?
・Sender side: resolver sin/cos signals A/D conversion ---> error correction ----> ZigBee,BT, WiFi transmission
・Reciever side: ZigBee,BT, WiFi recievering signals ----> signals recovery ----> D/A conversion ---> control board
Of course, a short delay between the sender the reciever sides is expected.
I will very appreciate your helps.
Thank you!