Part Number: CC2652P7
Other Parts Discussed in Thread: CC1352P7, SYSCONFIG
Hi team,
My customer is evaluating CC2652P7 for Matter RCP. Below list some questions. Please help clarify.
1. for HW schematic design, which reference design should be used ?
Inside CC2652P7 data sheet, it list two reference design. Customer want to put 20dBm on 2.4G. Which one is suitable ?

2. Which EVM is ok for SW development ?
LP-CC1352P7-1 or LP-CC1352P7-4
3.which example project for RCP FW .
Inside SDK/example/rtos, there are below two folder. However, only LP_CC1352P7_4 has Thread examples.
LP_CC1352P7_1
LP_CC1352P7_4
4. If customer want to use PTA (coexist with WiFi), could they use sysconfig to enable PTA and modify 3 wires pins ?