Hi,
We are planning to port our TI-15.4/900MHz based application to Zigbee/2.4GHz due to lack of mesh network implementation in that stack, have a few general questions:
1) Maximum allowed transmission power allowed to pass FCC certification
CFR Title 47 15.247 states that the transmission power can go up to 1watt if frequency hopping or digital modulation is utilized. Apparently TI zstack doesn't implement frequency hopping for 2.4GHz radios. So my questions here are:
1a): does ZStack implement some sort of digital modulation? I assume DSSS in the Phy Type means some sort of digital modulation.
1b) does 1watt translate to 20dBm in CC2652P launchpad based application? Any other factor to consider except reducing TX power for higher frequency channels as stated in user guild?
2) Power consumption of end device
We have very good power consumption numbers with CC13-90 radios when they are properly configured. My question here is: are power consumption of sleepy zed similar to sensor nodes in TI-15.4/Sub GHz? I tried to find some test results of example zed projects but I may have missed them.
3) Dynamically switch between sleepy end device and router
According to this post and other literature I have read so far, the role of a radio is determined at the time of firmware compilation, and TI doesn't provide out-of-box support for switching roles after firmware has been built and flashed into a radio.
But the linked post seems to imply it is possible to customize the firmware of a router and make role switch possible. Can someone confirm if this true? I can see this feature useful for our application, and if true, may put it on the list.
4) Maximum number of devices in a network
The default number of maximum number of device is 20, and 40 for TC link keys, with a theoretic limit at 65536. My question here is, what is the practical limit? We were advised to set maximum number of devices in a sbu-GHz network to 50. Is 50 or larger in ZStack network possible or advisable? Should we proportionally increase maximum number of TC link keys, NVS pages, and others?
Please advise,
Thanks,
ZL