Part Number: CC2531EMK
Other Parts Discussed in Thread: CC2531,
Dear all,
I am using the CC2531EMK (USB dongle) and rfusb_cc2531 example (from swrc088.zip examples code). I want to send 128 bytes from the PC to the usb dongle. By default the max length bytes are 64 bytes (USB 2.0) and if I send more than the 64 bytes from the PC, for example 76 bytes, I receive two frames with 64 + 12 bytes. I writting a protocol communication from PC to USB to RF and I want to send more than 64 bytes, that is 76 bytes. In the reference manual, at page 182, is specified that endpoints supports from 8 - 512 bytes, even with a FIFO up to 1024 bytes.
Since I am not an expert of USB, is there some way to increase to send more than 64 bytes (76 or 128 or more) in a single frame? I have tried to modify the file "usb_hid_descriptor.s51" but it doesn't work.
Please, is there a configuration or example code to achieve this?
Thanks.
Joaquim.
RM: