Part Number: CC2674R10
Hi,
Here is my use-case :
- I want to use the CC2674R10 in BLE only and then switch to Zigbee only in runtime.
- Once in Zigbee, I don't want the BLE stack / radio to have any impact on Zigbee and vice versa.
Questions :
- Is there a way (API?) to start & stop the BLE or Zigbee stack ?
- If no, should DMM be used by setting BLE / Zigbee in block mode ?
"A blocked stack will still be able to schedule commands and the current policy and GPT will be used to make scheduling decisions. This means that while a stack might have a blocking constraint set, it could still impact radio access for the other stack. This would happen in case the blocked stack’s radio commands is scheduled into the future (more then a few ms) while also being considered to be of higher priority."
- Is there a known settings (policy table, GPT..) where we will be sure that BLE does not impact ZIgbee when blocked and Zigbee won't impact BLE when blocked ?
Regards,
Geoffrey