Hi,
I couldn't find any example programs for SSED. Is it possible to run the CSL configuration in CC2652PSIP module to configure it as SSED?. If yes, please update how to do that. Thanks in advance.
regards,
Sudheesh U G
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I couldn't find any example programs for SSED. Is it possible to run the CSL configuration in CC2652PSIP module to configure it as SSED?. If yes, please update how to do that. Thanks in advance.
regards,
Sudheesh U G
Hi,
CSL should be enabled by default: https://github.com/search?q=repo%3ATexasInstruments%2Fot-ti+csl&type=code
And CC2652PSIP is also a supported board: https://github.com/TexasInstruments/ot-ti/blob/release/thread-1.3-certification-support/script/build#L60
Thanks,
Toby
Hi,
Thanks for the reply. Can I use the temperature sensor example for checking the CSL configurations?. I have set the following values in the temperature sensor program. But working of the CSL could not be verified.
#define OPENTHREAD_CONFIG_MAC_CSL_RECEIVER_ENABLE 1
#define OPENTHREAD_CONFIG_MAC_CSL_TRANSMITTER_ENABLE 1
#define OPENTHREAD_CONFIG_MAC_CSL_AUTO_SYNC_ENABLE 1
#define OPENTHREAD_CONFIG_MAC_CSL_MIN_PERIOD 10 //millisecond
#define OPENTHREAD_CONFIG_MAC_CSL_MAX_TIMEOUT 10000 //seconds
#define OPENTHREAD_CONFIG_CSL_TIMEOUT 100 //seconds
#define OPENTHREAD_CONFIG_MAC_CSL_DEBUG_ENABLE 0
#define OPENTHREAD_CONFIG_CSL_RECEIVE_TIME_AHEAD 320 //microseconds
#define OPENTHREAD_CONFIG_CSL_MIN_RECEIVE_ON 356 * 16
#define TIOP_CONFIG_POLL_PERIOD 60000
#define TIOP_TEMPSENSOR_REPORTING_INTERVAL 60000
The energy trace graph is shown below. But CSL pulses are not found.
I'll try to reproduce this on my end.
Please expect an update in 3 business days.
Hi Sudheesh U G,
Wanted to update you, I have not been able to reproduce the issue. Will try again next week.
Regards,
Toby
Hi Sudheesh U G,
In our next release of Thread (scheduled for end of April), it will be on https://github.com/TexasInstruments/ot-ti/tree/main and more easily enable support for CSL (through "TIOP_POWER_SSED"), including power measurement.
I recommend to use this once it is released, as it will contain latest updates for TI-OpenThread.
Thanks,
Toby