Part Number: LP-CC2651P3
Hello,
My project is based on zed sw which I am trying to connect to Zigbee2MQTT.
I want to disable the CUI and need to print on the screen. But when i disable CUI by Predefined symbol CUI_DISABLE, button press is not working.
/*********************************************************************
* @fn zclSampleSw_processKey
*
* @brief Key event handler function
*
* @param key - key to handle action for
* buttonEvents - event to handle action for
*
* @return none
*/
static void zclSampleSw_processKey(uint8_t key, Button_EventMask buttonEvents)
{
if (buttonEvents & Button_EV_CLICKED)
{
if(key == CONFIG_BTN_LEFT)
{
zstack_bdbStartCommissioningReq_t zstack_bdbStartCommissioningReq;
zstack_bdbStartCommissioningReq.commissioning_mode = zclSampleSw_BdbCommissioningModes;
Zstackapi_bdbStartCommissioningReq(appServiceTaskId,&zstack_bdbStartCommissioningReq);
}
if(key == CONFIG_BTN_RIGHT)
{
zstack_getZCLFrameCounterRsp_t rsp;
Zstackapi_getZCLFrameCounterReq(appServiceTaskId, &rsp);
zclGeneral_SendOnOff_CmdToggle( SAMPLESW_ENDPOINT, &zclSampleSw_DstAddr, FALSE, rsp.zclFrameCounter );
}
}
}
When I attempted to debug the code after disabling the CUI, pressing the button did not execute this function.
Is there any additional settings i need to do or do i need to make changes in the code ?
Thanks & Regards