Part Number: CC2651P3
Other Parts Discussed in Thread: Z-STACK,
Hi,
Can we adjust the wake up time for ZED example for 2 times a day?
Is that possible by adjusting POLL_RATE or any additional settings should be done?
Thanks & regards
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Anandhu,
The ZED is limited by a known issue, here is a reference from the Release Notes.
| ZIGBEE-1617 | Z-Stack sleepy ZED unexpectedly active when using large poll period values |
You can use a POLL_RATE value of 540000, or 9 minutes, which should not significantly affect your power consumption. This is the only time the ZED will be awake, unless data is queued by its parent or the ZED itself is transferring data.
Regards,
Ryan
What about Deep Sleep mode? Is it possible to wake up without an external interrupt from deep sleep?
There is no SRAM or register retention during shutdown mode, and only a pin edge, reset pin, or power-cycle will restart device activity. Since the previous device state is not retained, the CC2651P3 must restart the application which will require the ZED to rejoin the network. This requires several OTA packets which will consume more current than an in-network, one-time data request poll.
Regards,
Ryan