Part Number: CC2630
Tool/software:
I am encountering an issue with deployed devices where it is reporting reset_src=5 which is clock loss detect. These are happening on a large number of devices on sites we know to have fairly bad power. I suspect there is also a comorbidity where unexpected soft resets are being triggered with no obvious cause (we do not engage PRCM:WARMRESET.WR_TO_PINRESET) under similar conditions, but this is exceptionally hard to prove since the same bug that didn't engage that register also clears PRCM:WARMRESET.WDT_STAT.
The difficulty is that I have never reproduced either of these in a controlled setting. What I am trying to do right now is make either of the above conditions happen due to bad power conditions. Is there a way I can coax this into happening? I haven't had any success with simply under-volting with a DC power supply.