Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed the week of November 23.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2530-CC2592EM-RD: Unable to network

Part Number: CC2530-CC2592EM-RD
Other Parts Discussed in Thread: CC2591, CC2530, CC2592, Z-STACK

Tool/software:

Hi team,

We originally used the CC2530+CC2591 development board we bought, which can be used for networking and communication.
In the new version, we replaced the amplifier chip with CC2592 and used the officially recommended circuit: www.ti.com/.../CC2530-CC2592EM-RD
In the software, I have also made modifications to the corresponding en pin, OBSSEL4 -> OBSSEL0

The original circuit diagram and the new circuit diagram differ only in the en pin.
Original circuit pins: P1_1->PA-IN, P1_4 -> LAN_EN, P0_7 -> HGM.
Current circuit pins: P1_1->PA-IN, P1_0 -> LAN_EN, P0_7 -> HGM.
Then, they won't be able to form a network. If the BIAS resistor of CC2592 is removed to prevent it from working properly, the network will work again, but the distance will be very close, around 10CM.
If CC2592 is added, it will be completely impossible to network, which is strange. I don't know what the reason is.

Thanks & Best regards,

Jiahui