This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I tried to transmit/receive the data "123" by using CC2531 USB dongle through Serial Port Utility,
and i wanted CC2530(connected with SmartRF05EB) to receive/transmit the data.
and the data sent from CC2531 USB Dongle
The text "123" should be transfer into hex "31 32 33".
I have tried every setting on the serial port utility, and the data wasn't received correctly.
Is there any restricted format for CC2530 and CC2531 ??
How can i receive those data correctly??
Thank you !
1. You should use MT command for serial communication (http://e2e.ti.com/cfs-file.ashx/__key/communityserver-discussions-components-files/158/6758.Z_2D00_Stack-Monitor-and-Test-API.pdf) between your serial application and. CC253x.
2. You should use AF_DataReq to send data between CC2531 and CC2530.
Thanks for helping,Yikai.
I have solved my problem.
The baudrate was in wrong setting, it should be 38400, not 115200. The characters can be transmitted correctly now.
Thanks,Yikai.