This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi TI!
I have a zigbee network and the comercials devices can it join to network except the ZED example projects from Zstack (zed_sensortemperature, zed_devicelight, ...).
I did press the btn1 and nothing.
I did try to debbug the zed_sensortemperature example project and I see that the firware arrive to this code line 2654 :
events = 0; //This should not happen...
Any Idea about the problem, please?
Possible solutions plese.
Thank you very much. Best Regards
Hi YiKai Chen
Thank you very much for your answer,
I am using the CC1352 launchpad with simplelink_cc13x2_26x2_sdk_4_20_00_35. Please, could you suggest me how to check the setup correct channel?
Sincerely, thankou very much, best regards
You can change/set primary and secondary channels in CUI interface on UART console.
Hi YK Chen
Thank kou very much for your clear and fast answer!
Just right now I see the UART console, I didn't know about the UART console. The console UART showme the correct channel.
For to join it the device to the network, how I must to do?
1-) Enable the finding and binding via AURT console.
2-) Press BTN1
Only step 1-) is enough?
Sincerely, Tahnko very much
As I know, the default example only scan for channel 11 to join so you might to set primary/secondary channel to scan all zigbee channels. Otherwise, it might have trouble to join Zigbee network forms on other channels.