This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
I'm new to this CC2650 controller, i have to use this controller for my project "wireless temperature monitoring" using the Zigbee .
Is there is all the stacks for zigbee and the example codes for this controller is available? can i use this controller for my project are not.
if yes, which compiler i have to use for my development.
could any one please answer me.
Thank you!
Hi Varun,
It is possible to use Z-STACK-ARCHIVE HA 1.2.2a with IAR EWARM v7.40 for the CC2650 but this is not recommended due to a deprecated Zigbee Specification solution and lack of continued support. I would instead advise that you consider Z-Stack 3.0.2 for the CC2530 (EW8051 v10.20) or CC2538 (EWARM v8.22). Even more preferable is the CC2652R /P or CC1352R /P with SIMPLELINK-CC13X2-26X2-SDK as supported on the latest CCSTUDIO and IAR EWARM versions, this will offer the most up-to-date features and greatest hardware/software support. You can learn more about this platform by visiting TIREx.
Regards,
Ryan