Part Number: CC2652R
Other Parts Discussed in Thread: CC2530, ENERGYTRACE, SIMPLELINK-CC13X2-26X2-SDK, Z-STACK
Hi,
I tried performing energy trace on ZED_Sw example project and it is taking about 1mA with spikes of 6mA every 2 seconds. This is the out of the box example.
However, I checked the documents swra625b and swra478d and disabled the CUI. The current consumption still averages 500uA, (min: 200uA: max 6mA).
As per documentation, I was expecting a standby power of 1uA (already have cc2530 working at 1.5uA). Not sure if I am doing something wrong.
Please could you suggest how I can check.
The above measurements were done with EnergyTrace standalone mode.
Performing EnergyTrace++, shows that 100% time is spent at Deep Sleep Mode, so I am not sure why there is so much current consumption
Any advice would be useful
Thanks
Akhilesh