Other Parts Discussed in Thread: UCC27424-Q1, UCC27424
Hi all,
I'm using TMS3705 with UCC27424-Q1 amplifier (Configuration attached). The read range needs to be maximized up to 2m.
The progress up to now,
We used circular loop antennas with copper wires different gauges (Radius = 5cm) and able to have a read range of 30cm.
The questions,
1. What are the possible areas I can focus on to achieve it other than antenna design?
2. What are the possible types, orientations and significance that I should consider in antenna design (The antenna area should be less than 80cm X 5cm X 3cm)?
Thank you
Savinda