Hi,
I was wondering if the LMP92064 could sense something on its differential current sense inputs with this voltage range:
INCP pin: -60mV - 0V
INCN pin: 0V (GND)
Knowing that the minimum Vcm of the inputs is -200mV, it is not dangerous for the chip.
It is also possible for me to make it like that:
INCP pin: 0V (GND)
INCN pin: -60mV - 0V
Is the internal circuitry of the LMP92064 still capable of sensing the difference between the two inputs, even if one of those is negative?
Thank you!