Hello, my current control system, using a INA225AIDGKT with a 100V/V gain, is failling due to a step response delay near 25us, as is possible to see at attached picture. The magenta probe was directly on pins 1 and 8, and the blue probe on in 4, that isn't connect to external circuits or loads. The expected signal is the same of fig.24 from datasheet. What could be happening ?
Ricardo Urio