After reading the INA219 datasheet, I am unclear if the device goes into power down mode following a triggered conversion.
What does the device do after a triggered conversion? What is the power usage afterwards?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
After reading the INA219 datasheet, I am unclear if the device goes into power down mode following a triggered conversion.
What does the device do after a triggered conversion? What is the power usage afterwards?
Hello Reid,
Thank you for using the TI forums. I tested the INA219 at 5 V to see what current the device uses after each mode has been set, and these are the results:
MODE3 |
MODE2 |
MODE1 |
MODE |
Current (µA) |
Power (mW) |
0 |
0 |
0 |
Power-down |
65 |
0.325 |
0 |
0 |
1 |
Shunt voltage, triggered |
720 |
3.6 |
0 |
1 |
0 |
Bus voltage, triggered |
720 |
3.6 |
0 |
1 |
1 |
Shunt and bus, triggered |
720 |
3.6 |
1 |
0 |
0 |
ADC off (disabled) |
720 |
3.6 |
1 |
0 |
1 |
Shunt voltage, continuous |
742 |
3.71 |
1 |
1 |
0 |
Bus voltage, continuous |
730 |
3.65 |
1 |
1 |
1 |
Shunt and bus, continuous |
735 |
3.675 |
NOTE: This data was taken for one individual part and will vary for each device.
From this data it seems that after doing a triggered conversion the device goes into ADC off mode, not power down mode.