What does following graph tell? What is the differential input voltage?
What will be input bias current for the following circuit (LM111)? Voltage at Non-Inverting Pin = -8.5V (Vref LTP) & -9.5V (Vref UTP)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
What does following graph tell? What is the differential input voltage?
What will be input bias current for the following circuit (LM111)? Voltage at Non-Inverting Pin = -8.5V (Vref LTP) & -9.5V (Vref UTP)
Kamlesh,
Your images/attachments did not show. Please try again.
Sir,
Thanks a lot for your answer.
I am trying to have LTP and UTP for following circuit as -9.5 and -8.5 which is coming as expected at non-inverting input. However, output is changing state when input crosses reference at non-inverting terminal+100mV
What could be the reasons for this 100mV offset?
LM111 comparator is used in the circuit
(Pull up resistor for LM111 is not shown in the above circuit)
Kamlesh,
I need a little more information.
What is VCC- (pin 4) and VCC+ (pin 8) voltages?
Kamlesh,
Those supply voltages are good for the input voltage used.
I expect the issue is addressed here in your other post.
http://e2e.ti.com/support/amplifiers/etc_amplifiers__other_linear/f/18/t/364930.aspx
Sir,
I could get rid of noise by using shielded DMM probes. However I could not get rid of 100 mV offset between Non-Inverting and Inverting Pin of LM111 comparato while achieving LTP of -10V and UTP of -9V.
Could it be because of high input resistance value of 510 kilo-ohms used in between Inverting terminal and ground? Could Input bias current create offsets due to unmatched externally resistances at Inverting and Non-Inverting terminal of LM111?
Also. Input signal is given though diode as shown in the following diagram. Could diode non-linearity be the reason behind offset of 100mV between Inverting and Non-Inverting terminal of op-amp while achieving LTP of -10V and UTP of -9V?
Kamlesh,
The diode does affect the voltage at 'input' node, but the voltage offset at the opamp input should be about equal at switch (within the input noise amplitude).
I believe that supply voltage was close to +/-15V. Output voltage is 0V and 12V.
Is +Ve a good -9V and -10V?
Are the -Ve switch points -9.1V and -9.9V? or is the 100mV shift in a different direction?