I built this circuit on my board and have noticed some current discrepancies.
With no MCU/ADC load on the 5V Vreg line other than the resistor into IIN, the XTR117 is behaving normally. I can measure 5V DC at Vreg and the IOUT is what I am expecting.
Powering the MCU/ADC with a bench top power supply and a current meter, but completely isolated from the XTR117 circuit, i.e. cut the traces so the two portions are completely isolated from each other, I get a reading of 5mA at 5V.
Introduce the XTR117 to the MCU/ADC circuit and power up with 24VDC bench supply and I get a reading of 12mA at 24VDC. 5V Vreg reads 4.71V
Remove 24VDC bench power supply and power the 5V directly with a bench power supply. This time without isolating the XTR117 from the MCU/ADC and I'm reading close to 60mA at 5VDC.
What is going on when I join the MCU/ADC to the XTR117? Why is the current consumption all of a sudden jumping up to 60mA at 5V? Too much capacitance with the MCU/ADC capacitors? I tried removing the larger caps and still no changes.