I am using an LF 356 in the non inverting mode. I have connected the offset null ckt as suggested in the TI data sheet with the wiper of the null pot connected to the +12V supply. I am using -12V, Vee on pin 4. The input voltage is 0 - 5 VDC. The gain is nearly 1. The amplifier is working but turning the 25k offset null pot has no effect on the output.
Does the offset null circuit (pins 1 and 5) not work for the non inverting ckt? For non inverting should I connect the wiper to Vee, -12V? My input voltage will never go negative. Should I use ground instead of -12V, Vee on pin 4?