I am using OPA541SM...note the SM portion. The 8 pin package. In the datasheet there is no reference in the datasheet as to which pins are for which function. There is a reference to the 11-pin package pin out functions but not the 8 pin. I hope I missed something simple because this is datasheet 101....Can someone please tell me which pins are for which function?