LMV7119
For this device, I need help in calculating the decrease in the life of this part if the operating supply voltage is close to its maximum allowable operating voltage. We have a supply voltage derating of 80%. So, the derated supply voltage is 4.4V (80% of 5.5V rated) but the operating supply voltage is 5.0V. Is there a formula that I can use ? Is there some other way to calculate the life? Does the part run hotter at higher supply voltages? If so, can that be calculated?
Thanks,
Jef