Hi,
I don't get the use of AFE in DC PLC design. (it is also used in the 24 V DC PLC reference design from TI)
i came across a post saying that AFE is used because it has a DAC and analog filtering , PGA and power amplifier that can help put out high peak-to-peak PLC signals to the power line.
1)what is meant by "peak- to- peak signals to the power line."?
2) why do i need analog filtering when all AFE does is put my "MODULATED" data over the power line (master side) and extract "MODULATED" data and give the same to the micro controller (slave side) , clearly is not doing demodulating. (MCU does demodulation, doesn't it?)
3) AFE031 data sheet says it has zero crossing detectors also, but doesn't say what is their use , i doubt why does it need them when demodulation is not happening in AFE?
4) Digital communication in binary level (0,1) is less error prone while decoding is what i think and DAC adds more levels (more than 2 symbols symbols) , how is this profitable? (is this what he meant by saying peak-to-peak in question 1 )
Thanks in advance