I have a requirement for opamp that the input is from 60 nA to 120 uA and ,I need 0 to 3 volt output .
Any circuit recommendation ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Parviz,
60nA to 120uA is right on the edge of ~3.5 decades of input range (60-600nA, 600nA-6uA, 6-60uA, 60-120uA) which is usually right at the far end of what can be accomplished with a linear solution.
We suggest trying the circuit configuration shown the TI Circuit linked below. The circuit is described and design steps are provided on how to set the input to output transfer function as well how to select which bandwidth op amp you'll need.
Attached is the schematic , my result is not as linear as I want , can you make some comments please
Hello Parviz,
If we assume that the OPA320 output is lightly loaded, then the output swing range will be from about +10 mV to +4.990 V, for Vs = +5 V.Using a 100 k feedback resistor with the OPA320 the input current range would be limited to 100 nA on the low end, and 50 uA on the high end.Certainly that is a narrower range than the 6 nA to 120 uA you are attempting to accommodate with your design.
Maintaining a linear output voltage in relation to a linear input current will require keeping the output from swinging into the rails as previoulsy discussed. Applying a small common-mode voltage (VCM) to the non-inverting input, and then setting the transimpedance gain so that the output stays within the linear range will accomplish this task. Shown below is a TINA-TI simulation circuit with the OPA320 configured for +0.25 V VCM, and the transimpedance gain set to 37.5 kV/A. The output will then have a range from about +0.25 V to +4.75 V. Both linear and log plots for output voltage vs input current are shown.
If you think you would like to consider a log amplifier for the application take a look at the LOG114. It is very versatile and easy to apply. Here is the link to the LOG114 datasheet:
Regards, Thomas
Precision Amplifiers Applications Engineering