Feedback on "6.1 TI Precision Labs - Op Amps: Slew Rate 1"
Hi,
First of all, thank you for offering this kind of great Op Amps seminar online for free of charge.
These are really helpful for me and I would like to thank all the member who work for this seminar.
I have quick feedback on the course of Slew Rate 1.
We have a slide "Simulate Slew Rate - OPA2188" on page 7, and it seems SR is calculated with Vout from the range of 10%(-904mV) to 90%(899mV)
However, since Vout is 1Vpeak (2Vpp), if we use 10%/90%, then SR should be calculated from 10%(-800mV) to 90%(800mV).
Of course, the answer is still same (0.8V/us), however, if there is a trick behind, just let me know!
Thanks,
Ken