This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA4317: opa4317

Part Number: OPA4317

As above snapshot VOS is given at VS=5V. What are the min and maximum values for VS=3.3V.

Need for -40degC to 125 degC temperature range

  • Yashashree,

    The OPA4317 Vos specifications apply across the entire range of supply voltage and temperature.  Thus, while the maximum/minimum +/-90uV limit applies from 1.8V to 5.5V specified supply voltage at 25C, the max/min limit of +/-100uV also includes temperature variation from -40C to 125C.