Other Parts Discussed in Thread: LM358, TINA-TI
Hello,
customer has simulation problems with the TLV172 PSPICE model (see attachment). Btw, the lower LM358 reaches this simulation but not the needed values.
Regards, HolgerTLV172_model_problem.docx
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
customer has simulation problems with the TLV172 PSPICE model (see attachment). Btw, the lower LM358 reaches this simulation but not the needed values.
Regards, HolgerTLV172_model_problem.docx
Hello,
attached you find the TLV172 (as differential amplifier) schematic and settings. He wants a single static (DC) simulation.
Regards, Holger
Hi Holger,
I was able to put the circuit into Cadence and didn't see any issues with the model. Everything convergences and simulates well. After reviewing the information you provided me from the customer, I saw that the simulator is complaining about not having a 0V ground node. I recommend that the customer change the ground symbol in their circuit to one which has a 0 next to it.
This question is about the TLV172, but the attachment show the LM358 being used, which is a model that is old and unreliable. Which model is actually being used?
Please see the attached project files - have your customer try them and see if they work.
Thanks,
Paul