Hello,
I am using the INA233 in a noisy power supply application and am having trouble communicating with the INA233 at hot temperatures (85degC). One aspect I noticed where the INA233 differs from other PMBus chips is the logic low threshold level. The INA233 has a maximum 0.4V logic low threshold level whereas other PMBus chips may have a 0.8V maximum logic low level. My hypothesis at this time is that the logic low level threshold is drifting over temperature and the noise in the system is exceeding that threshold, resulting in failed communication. So, I have two questions:
- Are communication problems with the INA233 over temperature a known issue?
- Can you provide data / graphs of the logic level threshold drift over operating temperature?
Any insight would be helpful. Thanks.