I need a higher output voltage and fast settling, I was wondering if the ths3491 spice model would simulate a circuit like the one shown below accurately when driving the power rails with another amplifier. Also, any general comments about a design for higher voltage with fast settling would be appreciated if there was a different topology that seemed better suited or general application information / tips on using the ths3491 in a configuration like the one shown below to get ~2x output swing.
Thanks in advance!