Other Parts Discussed in Thread: THS4303
Dear Sir,
Application : We have a sensor for counting micron size particle which comprises of two pairs of electrodes. The 2.5V sin wave modulating signal is supplied to both pair of electrode and whenever the particle is present between any two pairs of electrode there is change in the current
Methodology :. Currently we are using THS4303 for converting the current coming from the electrode into the voltage. The difference of voltage between the electrodes is sensed using the THS4130. However, the current circuit is giving some unwanted frequency when the signal is demodulated. The peaks due to the particles are quite clear but with the unknown frequency. I am attaching schematic , block diagram and out put from the board.
Isssue : As you can see there are spurious frequencies. In the video you will see that, there is some constant frequency on which on our signal( the peaks you see are the events) is riding
Please let us know how to troubleshootTI query.rar