This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMH3401: Offset adjust

Guru 20090 points
Part Number: LMH3401
Other Parts Discussed in Thread: TINA-TI

Hello,

If VCM = 1.7 V and Vref = + 10 mV in the circuit of Figure 54, will the following output be obtained?

Vout + = + 1.710 V = + 1.700 V (CM) + 0.010 V (Vref)
Vout - = + 1.690 V = + 1.700 V (CM) - 0.010 V (Vref).

Best Regards,
Ryuji

  • Hello,

    I would like to add the offset to the VCM.
    If the above method is not used, please let me know application example for add the offset.

    Best Regards,
    Ryuji
  • Hi Ryuji,

    Yes, you could use the above method to add the offset to the input common mode. But, you need to be careful with the applied input offset as it will be an amplified offset at the output. So, a 10mV input offset will show up as 32mV offset at the output. You could simulate this in TINA-TI as below using DC analysis.

    Attached TINA-TI schematic for the same: LMH3401_InputOffset.TSC

    Best Regards,

    Rohit