Hello.
In the data sheet, there is 40uVpp, 0.1-1MHz.
I tried to get this number from the Noise density graph, but failed. Attached my calculations, based on you “Lecture Manual”.
Data from the data sheet:
Input Voltage Noise, f = 0.1Hz to 1MHz 40µVPP
From the Noise density graph:
enf=0.3µV/√Hz at 10Hz
f0=10 Hz
ennormal= enf√ f0=0.3*√10=0.95µV/√Hz at 1Hz
fL=0.1 Hz , fH=1 MHz
enflicker= ennormal√(ln(fH/ fL))=0.95*√(ln(1M/ 0.1))= 0.95*√(ln(107))=0.95*√(ln(107))= 0.95*√(4)=3.8 µVrms
enflicker(pp)=6* enflicker=6*3.8=22.8 µVPP
Please advise where is my mistake.