Part Number: ONET2591TA
Hello. I was wondering if one could use the ONET2591TA with an apd reverse biased at 140 V and avoid using the filter pin by connecting it to ground. I was also wondering if there are any newer/better transimpedance amplifier circuits available for reaching above 1 GHz that would allow me to reverse bias the apd at 140 V. Thanks for the help.